<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPX5010DP offset and sensitivity strange values in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPX5010DP-offset-and-sensitivity-strange-values/m-p/1939305#M8443</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a MPX5010DP pressure sensor connected to an Arduino Uno.&lt;BR /&gt;Pin 1 (with the mark) on the&amp;nbsp;MPX5010DP is connected to Pin A0, Pin 2 is connected to Ground and Pin 3 to 5V on the Arduino.&amp;nbsp;&lt;BR /&gt;Without any pressure applied, the offset value is about 1.58 V.&lt;BR /&gt;The sensitivity is about 2.43 mV/mm H2O. These values does not match the datasheet values : 0.2 V for the offset, 4.413 mV/mm H2O for the sensitivity.&lt;BR /&gt;I can't see anything wrong with my setup.&lt;/P&gt;&lt;P&gt;Has anyone ever observed this kind of problem?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 20:49:33 GMT</pubDate>
    <dc:creator>jlvassent</dc:creator>
    <dc:date>2026-02-03T20:49:33Z</dc:date>
    <item>
      <title>MPX5010DP offset and sensitivity strange values</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010DP-offset-and-sensitivity-strange-values/m-p/1939305#M8443</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a MPX5010DP pressure sensor connected to an Arduino Uno.&lt;BR /&gt;Pin 1 (with the mark) on the&amp;nbsp;MPX5010DP is connected to Pin A0, Pin 2 is connected to Ground and Pin 3 to 5V on the Arduino.&amp;nbsp;&lt;BR /&gt;Without any pressure applied, the offset value is about 1.58 V.&lt;BR /&gt;The sensitivity is about 2.43 mV/mm H2O. These values does not match the datasheet values : 0.2 V for the offset, 4.413 mV/mm H2O for the sensitivity.&lt;BR /&gt;I can't see anything wrong with my setup.&lt;/P&gt;&lt;P&gt;Has anyone ever observed this kind of problem?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010DP-offset-and-sensitivity-strange-values/m-p/1939305#M8443</guid>
      <dc:creator>jlvassent</dc:creator>
      <dc:date>2026-02-03T20:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPX5010DP offset and sensitivity strange values</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010DP-offset-and-sensitivity-strange-values/m-p/1940673#M8449</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;These devices are very sensitive. To ensure optimal performance, we recommend implementing auto-zero according to the application note linked below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1636.pdf" target="_self"&gt;Implementing Auto-Zero for Integrated Pressure Sensors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 20:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010DP-offset-and-sensitivity-strange-values/m-p/1940673#M8449</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2024-08-26T20:48:49Z</dc:date>
    </item>
  </channel>
</rss>