<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: Re: FXAS2100 not going into 'active' state</title>
    <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326671#M844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Actually the FXAS21000 and particularly the &lt;A href="http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=PFXAS21000CQR&amp;amp;buyNow=true&amp;amp;fromSearch=true"&gt;PFXAS21000CQR&lt;/A&gt; is no longer manufactured and was removed from the portfolio. This product has been only available as a pre-production sample and on certain demo boards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;The FXAS21002 is an improved version of the FXAS21000. In the attached file you can find a basic comparison between these two versions including availability information. As you can notice, samples are expected to be available during this month. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;You can discuss sampling and the production timing directly with &lt;A href="mailto:Dan.Sadler@freescale.com"&gt;Dan Sadler&lt;/A&gt;, who is the product line manager for gyroscopes. &lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif;"&gt;There is also the &lt;/SPAN&gt;&lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4917.pdf" style="font-family: Helvetica, sans-serif;"&gt;AN4917&lt;/A&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif;"&gt; describing both hardware and software compatibility. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;As for the self-test, you are right that it only works in Active mode, my question was irrelevant in this case.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Sep 2014 08:41:45 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2014-09-03T08:41:45Z</dc:date>
    <item>
      <title>FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326668#M841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am using the FRDM-FXS-MULTI-B board to evaluate and prototype a product with a Parallax propellor MCU.&lt;/P&gt;&lt;P&gt;I have the FXOS8700CQ working and responding so the i2c code is solid.&lt;/P&gt;&lt;P&gt;I can read all of the registers on the FXAS21000 gyroscope and the boot complete flag does go to 1 after a hard reset.&lt;/P&gt;&lt;P&gt;The problem I am having is that I can not set the 'Active' or 'Ready' bits in CTRL_REG1. I can set other higher bits in that register but for some reason bits 0 &amp;amp; 1 do not toggle. When I set the ST (self test) bit, the data does not output as described in the cdocumentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Help?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Jim-&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:57:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326668#M841</guid>
      <dc:creator>jimmiller</dc:creator>
      <dc:date>2026-02-03T21:57:32Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326669#M842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;It is hard to say where the problem might be, I am able to set both Active and Ready bits individually or simultaneously as you can see on the following screenshots. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM style=": ; font-size: 10pt;"&gt;Writing 0x03 to the CTRL_REG1 register:&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45816iAB29AAE93544022B/image-size/large?v=v2&amp;amp;px=999" title="write.JPG.jpg" alt="write.JPG.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM&gt;Reading 0x03 from the CTRL_REG1 register:&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39959i6E5B781908C0ECCC/image-size/large?v=v2&amp;amp;px=999" title="read.JPG.jpg" alt="read.JPG.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Could you please post here similar screenshots illustrating both I&lt;SUP&gt;2&lt;/SUP&gt;C write and read operations with the CTRL_REG1 (0x13) register? It might be also useful to see your source code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;How does the output data change when you set the ST bit? Note that the self-test is not factory trimmed, so it is considered successful if the minimum magnitude of change (50 counts for all axes) is achieved.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;SPAN style="font-weight: inherit; font-style: italic; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;&lt;EM style="font-weight: inherit; font-family: inherit;"&gt;PS:&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space"&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-weight: inherit; font-style: italic; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Sep 2014 12:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326669#M842</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2014-09-01T12:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326670#M843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I Can send you logic captures when I get back to lab tomorrow. I'm doubting its the code though, it works for other registers, even the configuration register with the 'active' bit. I can also set low order bits on other registers.&lt;/P&gt;&lt;P&gt;Per your question,&amp;nbsp; the output does not change when I set the ST bit. I was thinking it can only output data when 'active' but that was an assumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I Ordered another FRDM board to compare, it seems like a hardware issue so when the new board arrives I can compare results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;who do I contact about supply Of this chip? DiGiKey tried to special order it for me and said they cant get it? We want to go into production in a few weeks, possibly sooner.&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;jim-&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Sep 2014 18:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326670#M843</guid>
      <dc:creator>jimmiller</dc:creator>
      <dc:date>2014-09-02T18:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: Re: FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326671#M844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Actually the FXAS21000 and particularly the &lt;A href="http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=PFXAS21000CQR&amp;amp;buyNow=true&amp;amp;fromSearch=true"&gt;PFXAS21000CQR&lt;/A&gt; is no longer manufactured and was removed from the portfolio. This product has been only available as a pre-production sample and on certain demo boards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;The FXAS21002 is an improved version of the FXAS21000. In the attached file you can find a basic comparison between these two versions including availability information. As you can notice, samples are expected to be available during this month. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;You can discuss sampling and the production timing directly with &lt;A href="mailto:Dan.Sadler@freescale.com"&gt;Dan Sadler&lt;/A&gt;, who is the product line manager for gyroscopes. &lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif;"&gt;There is also the &lt;/SPAN&gt;&lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4917.pdf" style="font-family: Helvetica, sans-serif;"&gt;AN4917&lt;/A&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif;"&gt; describing both hardware and software compatibility. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;As for the self-test, you are right that it only works in Active mode, my question was irrelevant in this case.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 08:41:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326671#M844</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2014-09-03T08:41:45Z</dc:date>
    </item>
    <item>
      <title>Re: Re: FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326672#M845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, sent email to Dan, thanks for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Below are the logic analyzer captures of the Write and subsequent read of register $13.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45827i096B58C9F7BC5260/image-size/large?v=v2&amp;amp;px=999" title="Reg$13Write.JPG.jpg" alt="Reg$13Write.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39961iC4D3FD648E9D7FF8/image-size/large?v=v2&amp;amp;px=999" title="Reg$13Read.JPG.jpg" alt="Reg$13Read.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 16:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326672#M845</guid>
      <dc:creator>jimmiller</dc:creator>
      <dc:date>2014-09-03T16:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS2100 not going into 'active' state</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326673#M846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, new board arrived and gyro works. Has a bad gyro.&lt;/P&gt;&lt;P&gt;THanks for responding.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Sep 2014 02:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS2100-not-going-into-active-state/m-p/326673#M846</guid>
      <dc:creator>jimmiller</dc:creator>
      <dc:date>2014-09-06T02:37:24Z</dc:date>
    </item>
  </channel>
</rss>