<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMPX2010GP issue with voltage output</title>
    <link>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1824604#M8026</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am using the MPX2010GP pressure sensor to measure drop in pressure from airflow across sports fabrics. We expect a pressure drop of around 100Pa. There is currently an issue with the analog voltage output from the Pin 2 of the sensor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The datasheet says that at max rated gauge pressure of 10kPa the voltage output should be 25mV, but when measured using an RS PRO digital multi-meter I get a value of ~2.8V. The bench power supply used to provide the 10V to Pin 3 of the sensor is from&amp;nbsp;TTI EL302 PSU 0-30V,2A. I have repeated this with another MPX2010GP to check the original is not faulty. Everything is connected using a breadboard and jumper wires for prototyping.&lt;/P&gt;&lt;P&gt;Please could someone let me know what the potential issue with sensor or set up is here.&lt;/P&gt;&lt;P&gt;Pin connections are:&lt;/P&gt;&lt;P&gt;Pin 1: (Power supply) GND&lt;/P&gt;&lt;P&gt;Pin 2: Multi-meter&lt;/P&gt;&lt;P&gt;Pin 3: +10V&lt;/P&gt;&lt;P&gt;Pin 4: GND&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:29:29 GMT</pubDate>
    <dc:creator>house_burn</dc:creator>
    <dc:date>2026-02-03T21:29:29Z</dc:date>
    <item>
      <title>MPX2010GP issue with voltage output</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1824604#M8026</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am using the MPX2010GP pressure sensor to measure drop in pressure from airflow across sports fabrics. We expect a pressure drop of around 100Pa. There is currently an issue with the analog voltage output from the Pin 2 of the sensor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The datasheet says that at max rated gauge pressure of 10kPa the voltage output should be 25mV, but when measured using an RS PRO digital multi-meter I get a value of ~2.8V. The bench power supply used to provide the 10V to Pin 3 of the sensor is from&amp;nbsp;TTI EL302 PSU 0-30V,2A. I have repeated this with another MPX2010GP to check the original is not faulty. Everything is connected using a breadboard and jumper wires for prototyping.&lt;/P&gt;&lt;P&gt;Please could someone let me know what the potential issue with sensor or set up is here.&lt;/P&gt;&lt;P&gt;Pin connections are:&lt;/P&gt;&lt;P&gt;Pin 1: (Power supply) GND&lt;/P&gt;&lt;P&gt;Pin 2: Multi-meter&lt;/P&gt;&lt;P&gt;Pin 3: +10V&lt;/P&gt;&lt;P&gt;Pin 4: GND&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1824604#M8026</guid>
      <dc:creator>house_burn</dc:creator>
      <dc:date>2026-02-03T21:29:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPX2010GP issue with voltage output</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1824940#M8028</link>
      <description>&lt;P&gt;Hi Sean,&lt;/P&gt;
&lt;P&gt;It seems you are measuring the voltage on +Vout (pin 2) with respect to GND.&lt;/P&gt;
&lt;P&gt;However, this is not correct, you should measure the differential voltage between +Vout (pin 2) and -Vout (pin 4).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 539px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267500i4CF02D78841F9717/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 08:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1824940#M8028</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-03-11T08:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: MPX2010GP issue with voltage output</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1825177#M8031</link>
      <description>Hi Tomas,&lt;BR /&gt;&lt;BR /&gt;For the MPX2010GP it is a single gauge pressure sensor that I am looking to measure the pressure at a specific point, in this case where would the Pin 4 connect to as it is not a differential output.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Sean</description>
      <pubDate>Mon, 11 Mar 2024 12:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1825177#M8031</guid>
      <dc:creator>house_burn</dc:creator>
      <dc:date>2024-03-11T12:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: MPX2010GP issue with voltage output</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1825188#M8032</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Sean,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please see the answer on this topic from my colleague &lt;A href="https://community.nxp.com/t5/Sensors/Setting-up-the-MPX2010DP-differential-pressure-transducer/m-p/802535" target="_self"&gt;here&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 12:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010GP-issue-with-voltage-output/m-p/1825188#M8032</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-03-11T12:57:06Z</dc:date>
    </item>
  </channel>
</rss>