<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTM88 external sensor in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1794890#M7881</link>
    <description>&lt;P&gt;Hello guys, I still got the question, if I want to add an external temperature sensor to the NTM88, but it has no IIC, is it posible to use the ADC that comes with the NTM88?&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jan 2024 20:42:15 GMT</pubDate>
    <dc:creator>Sebastian-Jaimes</dc:creator>
    <dc:date>2024-01-24T20:42:15Z</dc:date>
    <item>
      <title>NTM88 external sensor</title>
      <link>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1785488#M7826</link>
      <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I'll like to add a temperature sensor beside the one that this uC comes with. How can I do that? is there an option for one wire connection for interfacing a sensor like DS18B20? or how can i send a spi data to the NTM88 for RF transmitting (I'm thinking of connecting Low power uC with a sensor and sending it to the NTM88 via spi). Or the possibility to connect analog sensor to the NTM88.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1785488#M7826</guid>
      <dc:creator>Jpernia89</dc:creator>
      <dc:date>2026-02-03T21:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: NTM88 external sensor</title>
      <link>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1786972#M7829</link>
      <description>&lt;P&gt;We don't have one wire connection temp sensor,but IIC interface instead.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/sensors/i3c-ic-digital-temp-sensors:MC_31128" target="_blank"&gt;I3C/I²C Digital Temperature Sensors | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 07:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1786972#M7829</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-01-11T07:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: NTM88 external sensor</title>
      <link>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1794890#M7881</link>
      <description>&lt;P&gt;Hello guys, I still got the question, if I want to add an external temperature sensor to the NTM88, but it has no IIC, is it posible to use the ADC that comes with the NTM88?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 20:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NTM88-external-sensor/m-p/1794890#M7881</guid>
      <dc:creator>Sebastian-Jaimes</dc:creator>
      <dc:date>2024-01-24T20:42:15Z</dc:date>
    </item>
  </channel>
</rss>