<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pressure Sensor MPXM2051GST1 spec in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1790503#M7863</link>
    <description>&lt;P&gt;On revision 5 of the MPXM2051G specification, 22 April 2021, on page 5 the Linearity in Table 4 shows a min of -0.3 and a max of +3.0 %Vfss. The maximum of +3.0 % seems high. Is this spec correct?&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 20:49:13 GMT</pubDate>
    <dc:creator>Adam_WM</dc:creator>
    <dc:date>2026-02-03T20:49:13Z</dc:date>
    <item>
      <title>Pressure Sensor MPXM2051GST1 spec</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1790503#M7863</link>
      <description>&lt;P&gt;On revision 5 of the MPXM2051G specification, 22 April 2021, on page 5 the Linearity in Table 4 shows a min of -0.3 and a max of +3.0 %Vfss. The maximum of +3.0 % seems high. Is this spec correct?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1790503#M7863</guid>
      <dc:creator>Adam_WM</dc:creator>
      <dc:date>2026-02-03T20:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPXM2051GST1 spec</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1790796#M7865</link>
      <description>&lt;P&gt;Dear Adam,&lt;/P&gt;
&lt;P&gt;unfortunately yes. The MPXM2051GS has such high linearity error. If you want a similar gauge sensor with much better linearity error, you can use for example&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/MPX2050.pdf" target="_self"&gt;MPX2050&lt;/A&gt;, which has the linearity error +/-0.25%.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1705560081822.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258740iD9D595B023104952/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1705560081822.png" alt="JozefKozon_0-1705560081822.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JozefKozon_0-1705560081822.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please check this &lt;A href="https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR?category=c265_c231_c82" target="_self"&gt;link&lt;/A&gt; for other differential and gauge pressure sensors up to 115kPa.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jan 2024 06:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1790796#M7865</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-01-18T06:43:12Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPXM2051GST1 spec</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1791194#M7867</link>
      <description>&lt;P&gt;Jozef,&lt;/P&gt;&lt;P&gt;Thanks for the reply. Sorry to be a bother, but on Rev 4 of the MPXM2051G specification the Linearity is listed as -0.3% to +0.3%, page 4, table 3. This is also the case for revision 1, 2, and 3 of the MPXM2051G spec. Revision 4 of the spec is attached.&lt;/P&gt;&lt;P&gt;The revision history on the rev 5 specification also does not mention a change to the Linearity spec.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help with this.&lt;/P&gt;&lt;P&gt;Adam M&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jan 2024 15:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1791194#M7867</guid>
      <dc:creator>Adam_WM</dc:creator>
      <dc:date>2024-01-18T15:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPXM2051GST1 spec</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1791612#M7869</link>
      <description>&lt;P&gt;Dear Adam,&lt;/P&gt;&lt;P&gt;thank you for the research you have conducted. Due to the new information you shared I think yes, the max. linearity value is most probably 0.3%VFSS, not 3%VFSS. I have contacted an application engineer for confirming the correct value and asked to fix the mistake in the datasheet rev. 5 if the 0.3% is correct. I will let you know the answer from the application engineer.&lt;/P&gt;&lt;P&gt;With Best Regards,&lt;/P&gt;&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 05:54:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1791612#M7869</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-01-19T05:54:13Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPXM2051GST1 spec</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1792751#M7874</link>
      <description>&lt;P&gt;Dear Adam,&lt;/P&gt;
&lt;P&gt;the application engineer confirmed, that the max. linearity value is a typo and it should be 0.3%VFSS, not the &lt;SPAN&gt;not 3%VFSS.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 08:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPXM2051GST1-spec/m-p/1792751#M7874</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2024-01-22T08:09:22Z</dc:date>
    </item>
  </channel>
</rss>