<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Angle sensor development in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Angle-sensor-development/m-p/316018#M784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Start by reviewing following app. note AN3107 Measuring Tilt with Low-g Accelerometers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;page 4:&lt;/P&gt;&lt;P&gt;...A 12-bit ADC cuts 3.3V supply into 4095 steps of 0.8mV for each step. Therefore, by taking one ADC reading of the MMA6260Q again at 0g (0° of tilt for an x-axis device), would now result in the following:&lt;/P&gt;&lt;P&gt;0°: 1650mV + 0.8mV = 1650.8mV&lt;/P&gt;&lt;P&gt;90°: 2450mV + 0.8mV = 2450.8mV &lt;/P&gt;&lt;P&gt;This results in a 0.057 degree resolution at the highest sensitivity point (0°) and 1.63 degree resolution at the lowest sensitivity point (90°). However, for 0.8mV changes, the noise factor becomes the factor to consider during design. How much noise the system has will depend on how much resolution you can get with a higher bit count.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 14-bit ADC accelerometer can be proportional better.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jun 2014 11:26:17 GMT</pubDate>
    <dc:creator>Martin35804</dc:creator>
    <dc:date>2014-06-19T11:26:17Z</dc:date>
    <item>
      <title>Angle sensor development</title>
      <link>https://community.nxp.com/t5/Sensors/Angle-sensor-development/m-p/316017#M783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to build a angle sensor with the following brief spec.:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Range : +/- 30 deg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Accuracy : 0.1 deg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Resolution : 0.01 deg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The angle measured will be roll or pitch(one at a time) of a body. Would like to have some advise from the community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking for an interesting discussion&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 13:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Angle-sensor-development/m-p/316017#M783</guid>
      <dc:creator>Sri10</dc:creator>
      <dc:date>2014-06-09T13:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Angle sensor development</title>
      <link>https://community.nxp.com/t5/Sensors/Angle-sensor-development/m-p/316018#M784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Start by reviewing following app. note AN3107 Measuring Tilt with Low-g Accelerometers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;http://cache.freescale.com/files/sensors/doc/app_note/AN3107.pdf?&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;page 4:&lt;/P&gt;&lt;P&gt;...A 12-bit ADC cuts 3.3V supply into 4095 steps of 0.8mV for each step. Therefore, by taking one ADC reading of the MMA6260Q again at 0g (0° of tilt for an x-axis device), would now result in the following:&lt;/P&gt;&lt;P&gt;0°: 1650mV + 0.8mV = 1650.8mV&lt;/P&gt;&lt;P&gt;90°: 2450mV + 0.8mV = 2450.8mV &lt;/P&gt;&lt;P&gt;This results in a 0.057 degree resolution at the highest sensitivity point (0°) and 1.63 degree resolution at the lowest sensitivity point (90°). However, for 0.8mV changes, the noise factor becomes the factor to consider during design. How much noise the system has will depend on how much resolution you can get with a higher bit count.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 14-bit ADC accelerometer can be proportional better.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jun 2014 11:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Angle-sensor-development/m-p/316018#M784</guid>
      <dc:creator>Martin35804</dc:creator>
      <dc:date>2014-06-19T11:26:17Z</dc:date>
    </item>
  </channel>
</rss>