<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MMA8451QR1</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8451QR1/m-p/1756101#M7707</link>
    <description>&lt;P&gt;Hello Terry,&lt;/P&gt;
&lt;P&gt;The INT pins can be configured using the PP_OD bit to be push-pull (PP_OD = 0 - default) or open drain (PP_OD = 1).&lt;/P&gt;
&lt;P&gt;The polarity of the INT pins can be configured using the IPOL bit. The default value is active low (IPOL = 0) meaning any interrupt event is signaled with a logical 0.&lt;/P&gt;
&lt;P&gt;PS: Note that the MMA8451QR1 is in “End of Life” status and we recommend either the FXLS8974CF or FXLS8967AF as a replacement.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 13 Nov 2023 08:02:23 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2023-11-13T08:02:23Z</dc:date>
    <item>
      <title>MMA8451QR1</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451QR1/m-p/1755797#M7702</link>
      <description>&lt;P&gt;Is there a block diagram for the pin structure of the INT pins?&amp;nbsp; Are they OD or totem pole? If there are internal PU/PD resistors what are the values?&lt;/P&gt;&lt;P&gt;I am trying to understand if there is a backfeed path from INT1 or INT2 back to VDD or VDDIO when VDD/VDDIO are high impedance and there is an external voltage on INT1 or INT2.&lt;/P&gt;&lt;P&gt;What kind of current can be tolerated in this condition?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451QR1/m-p/1755797#M7702</guid>
      <dc:creator>thipp</dc:creator>
      <dc:date>2026-02-03T20:52:24Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451QR1</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451QR1/m-p/1756101#M7707</link>
      <description>&lt;P&gt;Hello Terry,&lt;/P&gt;
&lt;P&gt;The INT pins can be configured using the PP_OD bit to be push-pull (PP_OD = 0 - default) or open drain (PP_OD = 1).&lt;/P&gt;
&lt;P&gt;The polarity of the INT pins can be configured using the IPOL bit. The default value is active low (IPOL = 0) meaning any interrupt event is signaled with a logical 0.&lt;/P&gt;
&lt;P&gt;PS: Note that the MMA8451QR1 is in “End of Life” status and we recommend either the FXLS8974CF or FXLS8967AF as a replacement.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 08:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451QR1/m-p/1756101#M7707</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-11-13T08:02:23Z</dc:date>
    </item>
  </channel>
</rss>