<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックExample code for the FXPS7550 available?</title>
    <link>https://community.nxp.com/t5/Sensors/Example-code-for-the-FXPS7550-available/m-p/1738574#M7645</link>
    <description>&lt;P&gt;I am trying to work with the FXPS7550 from a Raspberry Pi and it does not make any sense.&lt;/P&gt;&lt;P&gt;Note that I have connected other I2C devices to this machine before, without any issues.&lt;/P&gt;&lt;P&gt;Is there any example code for communicating with the sensor available?&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;The datasheet, sadly, raises more questions than it explains things. For example:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In section 7.3.4.2, for the temperature calculation "T_LSB" is mentioned. What is this? The value read from 0Eh, or the value read from SNSDATA0 when DATATYPE0 is set to 1?&lt;/LI&gt;&lt;LI&gt;Why is the temperature register value ranging from 13 to 250 on consequent reads? Shouldn’t the temperature stay relatively constant when the sensor is running in air?&lt;/LI&gt;&lt;LI&gt;What is the difference between SNSDATA0 and SNSDATA1? The datasheet just states that both registers contain pressure data, but what is the difference?&lt;/LI&gt;&lt;LI&gt;Where do the values come from / what do the variables mean in equation (4)? Is PABS_LSB the data read from the pressure register? If so, is it from SNSDATA0 or SNSDATA1? With both I get around 300kPa pressure, which does not seem right when the sensor is running in air.&lt;/LI&gt;&lt;LI&gt;Shouldn’t the pressure calibration value in register 0x4C, 0x4D be constant? When I read from it I get a different value every time.&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:35:15 GMT</pubDate>
    <dc:creator>ab4</dc:creator>
    <dc:date>2026-02-03T21:35:15Z</dc:date>
    <item>
      <title>Example code for the FXPS7550 available?</title>
      <link>https://community.nxp.com/t5/Sensors/Example-code-for-the-FXPS7550-available/m-p/1738574#M7645</link>
      <description>&lt;P&gt;I am trying to work with the FXPS7550 from a Raspberry Pi and it does not make any sense.&lt;/P&gt;&lt;P&gt;Note that I have connected other I2C devices to this machine before, without any issues.&lt;/P&gt;&lt;P&gt;Is there any example code for communicating with the sensor available?&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;The datasheet, sadly, raises more questions than it explains things. For example:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In section 7.3.4.2, for the temperature calculation "T_LSB" is mentioned. What is this? The value read from 0Eh, or the value read from SNSDATA0 when DATATYPE0 is set to 1?&lt;/LI&gt;&lt;LI&gt;Why is the temperature register value ranging from 13 to 250 on consequent reads? Shouldn’t the temperature stay relatively constant when the sensor is running in air?&lt;/LI&gt;&lt;LI&gt;What is the difference between SNSDATA0 and SNSDATA1? The datasheet just states that both registers contain pressure data, but what is the difference?&lt;/LI&gt;&lt;LI&gt;Where do the values come from / what do the variables mean in equation (4)? Is PABS_LSB the data read from the pressure register? If so, is it from SNSDATA0 or SNSDATA1? With both I get around 300kPa pressure, which does not seem right when the sensor is running in air.&lt;/LI&gt;&lt;LI&gt;Shouldn’t the pressure calibration value in register 0x4C, 0x4D be constant? When I read from it I get a different value every time.&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Example-code-for-the-FXPS7550-available/m-p/1738574#M7645</guid>
      <dc:creator>ab4</dc:creator>
      <dc:date>2026-02-03T21:35:15Z</dc:date>
    </item>
    <item>
      <title>Re: Example code for the FXPS7550 available?</title>
      <link>https://community.nxp.com/t5/Sensors/Example-code-for-the-FXPS7550-available/m-p/1738623#M7646</link>
      <description>&lt;P&gt;Dear Philipp,&lt;/P&gt;
&lt;P&gt;please find driver for the FXPS7xxx family in this &lt;A href="https://www.nxp.com/design/sensor-developer-resources/sensor-sw-component-library/sensor-drivers-for-nxp-sensors:SENSOR-DRIVERS#downloads" target="_self"&gt;link&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1697111136204.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244828i71B4D3E01D50BE32/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1697111136204.png" alt="JozefKozon_0-1697111136204.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 11:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Example-code-for-the-FXPS7550-available/m-p/1738623#M7646</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-10-12T11:45:49Z</dc:date>
    </item>
  </channel>
</rss>