<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No module named cli.cli - ssscli SE05X MW in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/No-module-named-cli-cli-ssscli-SE05X-MW/m-p/1735842#M7635</link>
    <description>&lt;P&gt;I'm trying to run ssscli from Plug and Trust MW, i've followed the documentation for install che cli and i'm stuck into this error. I've installed PyCli&amp;nbsp; an the error from "No module named 'cli'" become this:&lt;/P&gt;&lt;P&gt;File "&amp;lt;frozen runpy&amp;gt;", line 198, in _run_module_as_main&lt;BR /&gt;File "&amp;lt;frozen runpy&amp;gt;", line 88, in _run_code&lt;/P&gt;&lt;P&gt;File "C:\Users\%USER%\AppData\Roaming\Python\Python311-32\Scripts\ssscli.exe\__main__.py", line 4, in &amp;lt;module&amp;gt;&lt;BR /&gt;ModuleNotFoundError: No module named 'cli.cli'&lt;/P&gt;&lt;P&gt;Somebody have any solution?&lt;/P&gt;</description>
    <pubDate>Mon, 09 Oct 2023 14:25:06 GMT</pubDate>
    <dc:creator>WorkerEmbedded</dc:creator>
    <dc:date>2023-10-09T14:25:06Z</dc:date>
    <item>
      <title>No module named cli.cli - ssscli SE05X MW</title>
      <link>https://community.nxp.com/t5/Sensors/No-module-named-cli-cli-ssscli-SE05X-MW/m-p/1735842#M7635</link>
      <description>&lt;P&gt;I'm trying to run ssscli from Plug and Trust MW, i've followed the documentation for install che cli and i'm stuck into this error. I've installed PyCli&amp;nbsp; an the error from "No module named 'cli'" become this:&lt;/P&gt;&lt;P&gt;File "&amp;lt;frozen runpy&amp;gt;", line 198, in _run_module_as_main&lt;BR /&gt;File "&amp;lt;frozen runpy&amp;gt;", line 88, in _run_code&lt;/P&gt;&lt;P&gt;File "C:\Users\%USER%\AppData\Roaming\Python\Python311-32\Scripts\ssscli.exe\__main__.py", line 4, in &amp;lt;module&amp;gt;&lt;BR /&gt;ModuleNotFoundError: No module named 'cli.cli'&lt;/P&gt;&lt;P&gt;Somebody have any solution?&lt;/P&gt;</description>
      <pubDate>Mon, 09 Oct 2023 14:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/No-module-named-cli-cli-ssscli-SE05X-MW/m-p/1735842#M7635</guid>
      <dc:creator>WorkerEmbedded</dc:creator>
      <dc:date>2023-10-09T14:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: No module named cli.cli - ssscli SE05X MW</title>
      <link>https://community.nxp.com/t5/Sensors/No-module-named-cli-cli-ssscli-SE05X-MW/m-p/1737264#M7643</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224071"&gt;@WorkerEmbedded&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Did you have the issue following the steps listed in&amp;nbsp;simw-top/doc/pycli/doc/pre-steps.html#windows ? If yes, can you tell me in which step the issue happened? Thanks for your patience!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 08:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/No-module-named-cli-cli-ssscli-SE05X-MW/m-p/1737264#M7643</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-10-11T08:04:29Z</dc:date>
    </item>
  </channel>
</rss>