<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 pressure sensor MPXV7002 temperature range</title>
    <link>https://community.nxp.com/t5/Sensors/pressure-sensor-MPXV7002-temperature-range/m-p/1687252#M7505</link>
    <description>&lt;P&gt;The pressure sensor MPXV7002 has following temperature ranges:&lt;/P&gt;&lt;P&gt;operating: TA +10...+60°C&lt;/P&gt;&lt;P&gt;Do may cause permanent damage if operating at -10°C...+9°C? [yes or no]&lt;/P&gt;&lt;P&gt;I can accept in my project that the error will increase outside of the compensated temperature range (+10...+60°C), but I cannot accept that the sensor will be permanent damaged, as stated in the datasheet (Table 4. Maximum Ratings, note [1]).&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:39:39 GMT</pubDate>
    <dc:creator>andreacelani</dc:creator>
    <dc:date>2026-02-03T23:39:39Z</dc:date>
    <item>
      <title>pressure sensor MPXV7002 temperature range</title>
      <link>https://community.nxp.com/t5/Sensors/pressure-sensor-MPXV7002-temperature-range/m-p/1687252#M7505</link>
      <description>&lt;P&gt;The pressure sensor MPXV7002 has following temperature ranges:&lt;/P&gt;&lt;P&gt;operating: TA +10...+60°C&lt;/P&gt;&lt;P&gt;Do may cause permanent damage if operating at -10°C...+9°C? [yes or no]&lt;/P&gt;&lt;P&gt;I can accept in my project that the error will increase outside of the compensated temperature range (+10...+60°C), but I cannot accept that the sensor will be permanent damaged, as stated in the datasheet (Table 4. Maximum Ratings, note [1]).&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:39:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/pressure-sensor-MPXV7002-temperature-range/m-p/1687252#M7505</guid>
      <dc:creator>andreacelani</dc:creator>
      <dc:date>2026-02-03T23:39:39Z</dc:date>
    </item>
    <item>
      <title>Re: pressure sensor MPXV7002 temperature range</title>
      <link>https://community.nxp.com/t5/Sensors/pressure-sensor-MPXV7002-temperature-range/m-p/1687357#M7506</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Andrea,&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;yes, you can use the MPXV7002DP outside of the compensated temperature range (TA +10...+60°C), from -30°C to 100°C without damage. But as you mentioned the error is increased outside of the compensated area and we cannot guarantee how much.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jul 2023 08:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/pressure-sensor-MPXV7002-temperature-range/m-p/1687357#M7506</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-07-13T08:41:12Z</dc:date>
    </item>
  </channel>
</rss>