<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 S32V234 Camera Sensor and Deserializer</title>
    <link>https://community.nxp.com/t5/Sensors/S32V234-Camera-Sensor-and-Deserializer/m-p/1564822#M7184</link>
    <description>&lt;P&gt;Current development environment and purpose:&lt;BR /&gt;1. The version number of the development board is: SVM_HD_S32V234_V2.0_20180110&lt;BR /&gt;2. We want to use the external frame sync mode to calculate the delay stability of the transmission link from the camera sensor to the DDR buffer.&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. Does the hardware support the external frame sync mode?&lt;BR /&gt;2. Which pin is the SOC connected to the MAX9286? Is there a schematic diagram of this part available?&lt;BR /&gt;3. If the hardware supports it, is there any corresponding document on the software for reference?&lt;BR /&gt;4. If the hardware does not support it, how can the jumper solve this problem?&lt;/P&gt;</description>
    <pubDate>Tue, 06 Dec 2022 02:13:26 GMT</pubDate>
    <dc:creator>rafe_ma</dc:creator>
    <dc:date>2022-12-06T02:13:26Z</dc:date>
    <item>
      <title>S32V234 Camera Sensor and Deserializer</title>
      <link>https://community.nxp.com/t5/Sensors/S32V234-Camera-Sensor-and-Deserializer/m-p/1564822#M7184</link>
      <description>&lt;P&gt;Current development environment and purpose:&lt;BR /&gt;1. The version number of the development board is: SVM_HD_S32V234_V2.0_20180110&lt;BR /&gt;2. We want to use the external frame sync mode to calculate the delay stability of the transmission link from the camera sensor to the DDR buffer.&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. Does the hardware support the external frame sync mode?&lt;BR /&gt;2. Which pin is the SOC connected to the MAX9286? Is there a schematic diagram of this part available?&lt;BR /&gt;3. If the hardware supports it, is there any corresponding document on the software for reference?&lt;BR /&gt;4. If the hardware does not support it, how can the jumper solve this problem?&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 02:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S32V234-Camera-Sensor-and-Deserializer/m-p/1564822#M7184</guid>
      <dc:creator>rafe_ma</dc:creator>
      <dc:date>2022-12-06T02:13:26Z</dc:date>
    </item>
  </channel>
</rss>