<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MM9Z1_638 Zero voltage and Zero Current in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MM9Z1-638-Zero-voltage-and-Zero-Current/m-p/1552463#M7165</link>
    <description>&lt;P&gt;Hi Mike,&lt;/P&gt;
&lt;P&gt;please refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12301.pdf" target="_blank"&gt;AN12301&lt;/A&gt;. There is a possibility of VSENSE, ISENSE and TSENSE calibration. In the section 5. is the description of the system calibration procedure.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
    <pubDate>Fri, 11 Nov 2022 07:54:29 GMT</pubDate>
    <dc:creator>JozefKozon</dc:creator>
    <dc:date>2022-11-11T07:54:29Z</dc:date>
    <item>
      <title>MM9Z1_638 Zero voltage and Zero Current</title>
      <link>https://community.nxp.com/t5/Sensors/MM9Z1-638-Zero-voltage-and-Zero-Current/m-p/1552365#M7164</link>
      <description>&lt;P&gt;Hi NXP partner&lt;/P&gt;&lt;P&gt;We use MM9Z1_638 to be battery junction box senor board.When we apply 0V and 0A to mm9z1_638 senor board A~H point which show test configuration file. We found mm9z1_638 report&amp;nbsp; is 0~1.2V and 0~0.1A through CANBUS. as attached file. How to etiminate the minor voltage and current when our voltage sensor point and current senor with 0V and 0A.&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Mike Liang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Nov 2022 03:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MM9Z1-638-Zero-voltage-and-Zero-Current/m-p/1552365#M7164</guid>
      <dc:creator>a852013777</dc:creator>
      <dc:date>2022-11-11T03:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1_638 Zero voltage and Zero Current</title>
      <link>https://community.nxp.com/t5/Sensors/MM9Z1-638-Zero-voltage-and-Zero-Current/m-p/1552463#M7165</link>
      <description>&lt;P&gt;Hi Mike,&lt;/P&gt;
&lt;P&gt;please refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12301.pdf" target="_blank"&gt;AN12301&lt;/A&gt;. There is a possibility of VSENSE, ISENSE and TSENSE calibration. In the section 5. is the description of the system calibration procedure.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 11 Nov 2022 07:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MM9Z1-638-Zero-voltage-and-Zero-Current/m-p/1552463#M7165</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2022-11-11T07:54:29Z</dc:date>
    </item>
  </channel>
</rss>