<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Generic CSI2 application for S32R45 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478251#M6964</link>
    <description>&lt;P&gt;We do not have a standalone CSI2 application as it needs a front-end to connect to.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to use it with another frontend, you can use the RF_Abstract/RFE driver source code as a reference/example for configuring and using the CSI2 driver for data acquisition.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tudor&lt;/P&gt;</description>
    <pubDate>Wed, 22 Jun 2022 14:39:54 GMT</pubDate>
    <dc:creator>b41937</dc:creator>
    <dc:date>2022-06-22T14:39:54Z</dc:date>
    <item>
      <title>Generic CSI2 application for S32R45</title>
      <link>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1477480#M6958</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We found out that, there is a CSI2 application in RSDK package specifically for TFE82XX. Is there any generic CSI2 application (or standalone CSI2 application)available for S32R45.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mufeeda P P&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 13:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1477480#M6958</guid>
      <dc:creator>Mufeeda_P_P</dc:creator>
      <dc:date>2022-06-21T13:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: Generic CSI2 application for S32R45</title>
      <link>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478239#M6962</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;The CSI2 driver is agnostic of the connected frontend. There are 2 applications in RSDK that exemplify in a similar manner how the CSI2 driver can be integrated: RFE Capture and Multi RFE example. Both use the CSI2 driver with TEF82XX frontend. RFE capture may be a better starting point as it only addresses data acquisition.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tudor&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 14:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478239#M6962</guid>
      <dc:creator>b41937</dc:creator>
      <dc:date>2022-06-22T14:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: Generic CSI2 application for S32R45</title>
      <link>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478247#M6963</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We checked these 2 applications in RSDK. But we want the standalone CSI2 application for receiving RAW data from the RADAR not for TEF82XX.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note : If not application, any standalone code to get the frame data in storage device is fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mufeeda P P&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 14:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478247#M6963</guid>
      <dc:creator>Mufeeda_P_P</dc:creator>
      <dc:date>2022-06-22T14:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: Generic CSI2 application for S32R45</title>
      <link>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478251#M6964</link>
      <description>&lt;P&gt;We do not have a standalone CSI2 application as it needs a front-end to connect to.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to use it with another frontend, you can use the RF_Abstract/RFE driver source code as a reference/example for configuring and using the CSI2 driver for data acquisition.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tudor&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 14:39:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Generic-CSI2-application-for-S32R45/m-p/1478251#M6964</guid>
      <dc:creator>b41937</dc:creator>
      <dc:date>2022-06-22T14:39:54Z</dc:date>
    </item>
  </channel>
</rss>