<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RISC-V EDUCATION in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455206#M6907</link>
    <description>&lt;P&gt;Which part do you mean for this topic?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 09 May 2022 22:13:48 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-05-09T22:13:48Z</dc:date>
    <item>
      <title>RISC-V EDUCATION</title>
      <link>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455189#M6906</link>
      <description>&lt;P&gt;IS THERE AN NEED FOR EDUCATION IN USING RISC-V&amp;nbsp; ISA&amp;nbsp; FOR SENSORS AND SOFTWARE REQUIREMENTS WITH THE POSSIBILITY OF NO FIRST ERROR? A TECHNIQUE?&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 20:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455189#M6906</guid>
      <dc:creator>CYBORGJ</dc:creator>
      <dc:date>2022-05-09T20:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: RISC-V EDUCATION</title>
      <link>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455206#M6907</link>
      <description>&lt;P&gt;Which part do you mean for this topic?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 22:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455206#M6907</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-05-09T22:13:48Z</dc:date>
    </item>
    <item>
      <title>Re: RISC-V EDUCATION</title>
      <link>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455906#M6909</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;since once I spent 8 hours developing a C program for a Texas Instruments launchpad that used SPI communication (which can be very intricate) I was successful. After that I realized the process can be standardized into a type of secretarial work procedure using a 3 step process which can then be used to create a no first error program to meet Software Requirements. Since some of the MEMS&amp;nbsp; are very useful, my process may be be a needed one?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thus, my process may be applicable to many different type of mems as I only used it for a specific&amp;nbsp; 3-axis magnetic MEMS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Tue, 10 May 2022 22:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/RISC-V-EDUCATION/m-p/1455906#M6909</guid>
      <dc:creator>CYBORGJ</dc:creator>
      <dc:date>2022-05-10T22:26:46Z</dc:date>
    </item>
  </channel>
</rss>