<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 MXP2300DT1 with Arduino</title>
    <link>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1412713#M6840</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am doing a very basic project that integrates the sensor&amp;nbsp;MXP2300DT1 with Arduino Adafruit feather M0 WiFI. On the Arduino IDE, I found only one library named: PRESSUREMPXNXP&amp;nbsp; which only defines the MPX500 series sensors. My question is:&amp;nbsp; Do you know if I can use this same library for the MXP2300DT1? Or is it any other library I can use?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks is advance!&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:36:02 GMT</pubDate>
    <dc:creator>anniemm</dc:creator>
    <dc:date>2026-02-03T21:36:02Z</dc:date>
    <item>
      <title>MXP2300DT1 with Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1412713#M6840</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am doing a very basic project that integrates the sensor&amp;nbsp;MXP2300DT1 with Arduino Adafruit feather M0 WiFI. On the Arduino IDE, I found only one library named: PRESSUREMPXNXP&amp;nbsp; which only defines the MPX500 series sensors. My question is:&amp;nbsp; Do you know if I can use this same library for the MXP2300DT1? Or is it any other library I can use?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks is advance!&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1412713#M6840</guid>
      <dc:creator>anniemm</dc:creator>
      <dc:date>2026-02-03T21:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: MXP2300DT1 with Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1413070#M6843</link>
      <description>&lt;P&gt;Hello Annie,&lt;/P&gt;
&lt;P&gt;I am not very familiar with the PRESSUREMPXNXP Arduino library, I would recommend you to post your question on the Arduino forum.&lt;/P&gt;
&lt;P&gt;However, the MXP2300DT1 is a non-amplified pressure sensor with a &amp;nbsp;differential output voltage in the range of few mV. It usually needs to be coupled with a differential amplifier to achieve a higher single ended output voltage.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 12:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1413070#M6843</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-02-14T12:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: MXP2300DT1 with Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1419319#M6848</link>
      <description>&lt;P&gt;Thanks for your answer. I figured out the Arduino part. But could you please tell me what would be the output of the sensor in mV for 40Kpa? Is it 3mV?&lt;/P&gt;&lt;P&gt;I already coupled it with an amplifier, but&amp;nbsp; I am not sure I am getting accurate data.&lt;/P&gt;&lt;P&gt;Do you have a recommendation for the type of amp I should use?&amp;nbsp;&lt;/P&gt;&lt;P&gt;As of now, I have this one:&amp;nbsp;&lt;A href="https://www.amazon.com/gp/product/B07YHYSXR6/ref=ppx_yo_dt_b_asin_title_o00_s00?ie=UTF8&amp;amp;psc=1" target="_blank"&gt;https://www.amazon.com/gp/product/B07YHYSXR6/ref=ppx_yo_dt_b_asin_title_o00_s00?ie=UTF8&amp;amp;psc=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I set it up so 4mV ---&amp;gt; 2V, but when I am testing the sensor I get all sorts of random measurements and I do not have a reference of Kpa to compare.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 18:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1419319#M6848</guid>
      <dc:creator>anniemm</dc:creator>
      <dc:date>2022-02-24T18:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: MXP2300DT1 with Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1535310#M7121</link>
      <description>&lt;P&gt;Because of my limited experience with the PRESSUREMPXNXP Arduino library, I suggest you ask your query on the official Arduino support forum.&lt;/P&gt;&lt;P&gt;The MXP2300DT1, on the other hand, is a non-amplified pressure sensor that produces a differential output voltage of only a few millivolts. Combining it with a differential amplifier is the standard method for increasing the single-ended output voltage. &lt;A href="https://marykayintouch.pics/" target="_self"&gt;MaryKayInTouch&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 05:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXP2300DT1-with-Arduino/m-p/1535310#M7121</guid>
      <dc:creator>youthconnect</dc:creator>
      <dc:date>2022-10-11T05:19:52Z</dc:date>
    </item>
  </channel>
</rss>