<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Getting started with MPXV6115V for Arduino in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Getting-started-with-MPXV6115V-for-Arduino/m-p/1407025#M6824</link>
    <description>&lt;P&gt;Hi James,&lt;/P&gt;
&lt;P&gt;It should be easy to connect this sensor to Arduino boards.&lt;/P&gt;
&lt;P&gt;It is a 5V, temperature compensated and calibrated vacuum pressure sensor. The full-scale output (&lt;SPAN&gt;no pressure difference between P1 and P2&lt;/SPAN&gt;) is typ. 4.6V and the output is 38.26mV per kPa.&amp;nbsp;&lt;SPAN&gt;Considering Arduino's typical 10-bit ADC powered at 5V, each ADC step corresponds to ~4.88mV (5V/1024) or 127.5Pa.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The pins are numbered as follows:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 365px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/169203i99F5169069C831B7/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So connect Arduino 5V to sensor pin 2. Arduino GND to sensor pin 3.&amp;nbsp;Arduino analog input (for example A0) to sensor pin 4.&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN&gt;Read the analog value and write it to the serial monitor:&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://docs.arduino.cc/built-in-examples/basics/ReadAnalogVoltage" target="_blank"&gt;http://arduino.cc/en/Tutorial/ReadAnalogVoltage&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If that is working, you can start to calculate the actual pressure.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 31 Jan 2022 10:39:29 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2022-01-31T10:39:29Z</dc:date>
    <item>
      <title>Getting started with MPXV6115V for Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/Getting-started-with-MPXV6115V-for-Arduino/m-p/1406860#M6823</link>
      <description>&lt;P&gt;I've just received a&amp;nbsp;&lt;SPAN&gt;MPXV6115V and am trying to use it to measure internal pressure of a suction device. There doesn't seem to be any resources on how to use this with an Arduino so I wanted to ask if anyone could provide a link to some example code or help with setting this sensor up? Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Getting-started-with-MPXV6115V-for-Arduino/m-p/1406860#M6823</guid>
      <dc:creator>jamesb4753</dc:creator>
      <dc:date>2026-02-03T20:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Getting started with MPXV6115V for Arduino</title>
      <link>https://community.nxp.com/t5/Sensors/Getting-started-with-MPXV6115V-for-Arduino/m-p/1407025#M6824</link>
      <description>&lt;P&gt;Hi James,&lt;/P&gt;
&lt;P&gt;It should be easy to connect this sensor to Arduino boards.&lt;/P&gt;
&lt;P&gt;It is a 5V, temperature compensated and calibrated vacuum pressure sensor. The full-scale output (&lt;SPAN&gt;no pressure difference between P1 and P2&lt;/SPAN&gt;) is typ. 4.6V and the output is 38.26mV per kPa.&amp;nbsp;&lt;SPAN&gt;Considering Arduino's typical 10-bit ADC powered at 5V, each ADC step corresponds to ~4.88mV (5V/1024) or 127.5Pa.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The pins are numbered as follows:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 365px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/169203i99F5169069C831B7/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So connect Arduino 5V to sensor pin 2. Arduino GND to sensor pin 3.&amp;nbsp;Arduino analog input (for example A0) to sensor pin 4.&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN&gt;Read the analog value and write it to the serial monitor:&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://docs.arduino.cc/built-in-examples/basics/ReadAnalogVoltage" target="_blank"&gt;http://arduino.cc/en/Tutorial/ReadAnalogVoltage&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If that is working, you can start to calculate the actual pressure.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jan 2022 10:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Getting-started-with-MPXV6115V-for-Arduino/m-p/1407025#M6824</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-01-31T10:39:29Z</dc:date>
    </item>
  </channel>
</rss>