<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPX5100 - Vacuum Measurement in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPX5100-Vacuum-Measurement/m-p/1380480#M6776</link>
    <description>&lt;P&gt;Hi Roberto,&lt;/P&gt;
&lt;P&gt;I believe you can use the MPX5100DP for this purpose.&amp;nbsp;As long as the pressure difference between P1 and P2 is less than 100kPa and P1&amp;gt;P2, there will be no issue.&lt;/P&gt;
&lt;P&gt;You can also consider using the &lt;A href="https://www.nxp.com/part/MPXV6115VC6U#/" target="_self"&gt;MPXV6115VC6U&lt;/A&gt; gauge vacuum sensor.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
    <pubDate>Thu, 02 Dec 2021 08:53:15 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2021-12-02T08:53:15Z</dc:date>
    <item>
      <title>MPX5100 - Vacuum Measurement</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5100-Vacuum-Measurement/m-p/1379720#M6771</link>
      <description>&lt;P&gt;Hi, I would like some information about the MPX5100DP sensor.&lt;/P&gt;&lt;P&gt;I need to perform a measurement on an electromedical equipment and this makes a vacuum inside suction cups that are attached to the patient.&lt;/P&gt;&lt;P&gt;The measurement range would be from 0kpa to -100kpa.&lt;/P&gt;&lt;P&gt;Could you use this sensor for this purpose?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5100-Vacuum-Measurement/m-p/1379720#M6771</guid>
      <dc:creator>WRGandolphini</dc:creator>
      <dc:date>2026-02-03T20:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: MPX5100 - Vacuum Measurement</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5100-Vacuum-Measurement/m-p/1380480#M6776</link>
      <description>&lt;P&gt;Hi Roberto,&lt;/P&gt;
&lt;P&gt;I believe you can use the MPX5100DP for this purpose.&amp;nbsp;As long as the pressure difference between P1 and P2 is less than 100kPa and P1&amp;gt;P2, there will be no issue.&lt;/P&gt;
&lt;P&gt;You can also consider using the &lt;A href="https://www.nxp.com/part/MPXV6115VC6U#/" target="_self"&gt;MPXV6115VC6U&lt;/A&gt; gauge vacuum sensor.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 08:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5100-Vacuum-Measurement/m-p/1380480#M6776</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-12-02T08:53:15Z</dc:date>
    </item>
  </channel>
</rss>