<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 MM9Z1 system calibration</title>
    <link>https://community.nxp.com/t5/Sensors/MM9Z1-system-calibration/m-p/1344490#M6707</link>
    <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;Dear support/community,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;as mentioned in the datasheet(MM9Z1_638D1), a&lt;/SPAN&gt;&amp;nbsp;system calibration should be performed on the system level to remove effects/errors introduced through device configuration, soldering, and external components. T&lt;/FONT&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;he calibration should be performed at ~25°C.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;My question is, does the temperature 25°C correspond to room temperature or Tsense chip temperature(ITS).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Shaojun&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 00:48:04 GMT</pubDate>
    <dc:creator>Shaojun</dc:creator>
    <dc:date>2021-09-23T00:48:04Z</dc:date>
    <item>
      <title>MM9Z1 system calibration</title>
      <link>https://community.nxp.com/t5/Sensors/MM9Z1-system-calibration/m-p/1344490#M6707</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;Dear support/community,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;as mentioned in the datasheet(MM9Z1_638D1), a&lt;/SPAN&gt;&amp;nbsp;system calibration should be performed on the system level to remove effects/errors introduced through device configuration, soldering, and external components. T&lt;/FONT&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;he calibration should be performed at ~25°C.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;My question is, does the temperature 25°C correspond to room temperature or Tsense chip temperature(ITS).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Shaojun&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 00:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MM9Z1-system-calibration/m-p/1344490#M6707</guid>
      <dc:creator>Shaojun</dc:creator>
      <dc:date>2021-09-23T00:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1 system calibration</title>
      <link>https://community.nxp.com/t5/Sensors/MM9Z1-system-calibration/m-p/1344933#M6708</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Shaojun,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;there is an application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN12301.pdf" target="_self"&gt;AN12301&lt;/A&gt; describing calibration processes of the MM9Z1 temperature sensor. The calibration should be performed at room temperature&amp;nbsp;&lt;SPAN&gt;~25°C. If the chip is unused for few hours the room temperature and ITS will be the same.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;With Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jozef&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 11:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MM9Z1-system-calibration/m-p/1344933#M6708</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-09-23T11:29:54Z</dc:date>
    </item>
  </channel>
</rss>