<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MMA8451Q Tilt</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Tilt/m-p/296701#M670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally meets self! &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I chose to integrate the method provided in this datasheet: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.analog.com/static/imported-files/application_notes/AN-1057.pdf"&gt;http://www.analog.com/static/imported-files/application_notes/AN-1057.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;On a PIC18 clocked at 8MHz, the computation time is 1.5ms, which is still reasonable. &lt;/P&gt;&lt;P&gt;Too bad, I have not found a solution to use the MMA8451Q with a interrupt, which would have saved me energy. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgards,&lt;/P&gt;&lt;P&gt;Gaétan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 May 2014 12:21:26 GMT</pubDate>
    <dc:creator>gaétanphilbiche</dc:creator>
    <dc:date>2014-05-14T12:21:26Z</dc:date>
    <item>
      <title>MMA8451Q Tilt</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Tilt/m-p/296700#M669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use a MMA8451Q to monitor a device that does not have to bend over x degrees to the vertical axis. Before I used a tilt switch CM1320-0 from Assemtech and wish to obtain the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To do this , I thought used to detect portrait/landscape integrated. But I realize doing my tests that this mode is not the same if you turn around the Z axis or if the Z axis is tilted up or down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Operation when turning around Z is perfect for my application, ideally I would have the same mode of operation on the other axis . But when I switch to the front ( Z down) , I have no hysteresis and backward (Z up) I hysteresis is too important! I tried to cheat the offset of the Z axis, but this is not enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if there is another solution that regularly read the MMA8451Q and make the angle calculation from the XYZ readings ? If there is no alternative , is there a sample source code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gaétan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-Tilt/m-p/296700#M669</guid>
      <dc:creator>gaétanphilbiche</dc:creator>
      <dc:date>2026-02-03T21:24:07Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q Tilt</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Tilt/m-p/296701#M670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally meets self! &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I chose to integrate the method provided in this datasheet: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.analog.com/static/imported-files/application_notes/AN-1057.pdf"&gt;http://www.analog.com/static/imported-files/application_notes/AN-1057.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;On a PIC18 clocked at 8MHz, the computation time is 1.5ms, which is still reasonable. &lt;/P&gt;&lt;P&gt;Too bad, I have not found a solution to use the MMA8451Q with a interrupt, which would have saved me energy. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgards,&lt;/P&gt;&lt;P&gt;Gaétan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 12:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-Tilt/m-p/296701#M670</guid>
      <dc:creator>gaétanphilbiche</dc:creator>
      <dc:date>2014-05-14T12:21:26Z</dc:date>
    </item>
  </channel>
</rss>