<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMXPV7007G drift</title>
    <link>https://community.nxp.com/t5/Sensors/MXPV7007G-drift/m-p/1287673#M6593</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using the MXPV7007G to measure negative pressure in the range 0 to -1000 Pa.&lt;/P&gt;&lt;P&gt;In normal cases the pressure is varying within this range frequented.&amp;nbsp; But at times there should be no change in pressure for several days. The sensor however reports an increase in negative pressure over time. A relatively constant change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Over 3 days for instance the sensor is reporting a change from -500 to -1000 Pa.&lt;/P&gt;&lt;P&gt;There is nothing in the system that I see could cause an increase in negative pressure.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I wonder if this could be due to sensor drift.&lt;/P&gt;&lt;P&gt;Any thoughts on this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:50:56 GMT</pubDate>
    <dc:creator>ThomasX</dc:creator>
    <dc:date>2026-02-03T21:50:56Z</dc:date>
    <item>
      <title>MXPV7007G drift</title>
      <link>https://community.nxp.com/t5/Sensors/MXPV7007G-drift/m-p/1287673#M6593</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using the MXPV7007G to measure negative pressure in the range 0 to -1000 Pa.&lt;/P&gt;&lt;P&gt;In normal cases the pressure is varying within this range frequented.&amp;nbsp; But at times there should be no change in pressure for several days. The sensor however reports an increase in negative pressure over time. A relatively constant change.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Over 3 days for instance the sensor is reporting a change from -500 to -1000 Pa.&lt;/P&gt;&lt;P&gt;There is nothing in the system that I see could cause an increase in negative pressure.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I wonder if this could be due to sensor drift.&lt;/P&gt;&lt;P&gt;Any thoughts on this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXPV7007G-drift/m-p/1287673#M6593</guid>
      <dc:creator>ThomasX</dc:creator>
      <dc:date>2026-02-03T21:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: MXPV7007G drift</title>
      <link>https://community.nxp.com/t5/Sensors/MXPV7007G-drift/m-p/1288077#M6595</link>
      <description>&lt;P&gt;Hi Thomas,&lt;/P&gt;
&lt;P&gt;please refer to the transfer function in the page 6. in the datasheet attached for the possible drift reasons.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1623054024710.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146385i454DE368B5259E05/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_2-1623054024710.png" alt="JozefKozon_2-1623054024710.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The pressure error is guarantied to be maximally 500Pa. So the output can change reflecting a change up to 500Pa without any reason, even if there is no change in the pressure applied.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1623053755374.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146383i421B2F072107C492/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1623053755374.png" alt="JozefKozon_0-1623053755374.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Then there is Temperature error factor. For the temperature from 0°C to 85°C, the temperature error factor is one, but for the temperature below 0°C up to -40°C the factor increases from 1 to 3. The same for the temperature above 85°C up to 125°C.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_1-1623053974471.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146384i1EF686D805A3CCC4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_1-1623053974471.png" alt="JozefKozon_1-1623053974471.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The device is ratiometric to Vs supply, meaning if there is a change in the Vs supply voltage it will reflect in the output voltage even if there is no change in the applied pressure or in the Temperature error factor.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_3-1623054187851.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146386i3A83547364D597FD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_3-1623054187851.png" alt="JozefKozon_3-1623054187851.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 08:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MXPV7007G-drift/m-p/1288077#M6595</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-06-07T08:24:03Z</dc:date>
    </item>
  </channel>
</rss>