<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMPXV7002 Reference Pressure</title>
    <link>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262369#M6519</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a quick question regarding the single port variants of the&amp;nbsp;MPXV7002 pressure sensors. I just wanted to confirm that these single port models are referencing port 1 pressure to the sensor's ambient pressure, and not an internal vacuum. It seems that the latter would exceed the device's maximum pressure rating of 75 kPa, but I just wanted to make sure. Thank you,&lt;/P&gt;&lt;P&gt;Austin&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:53:41 GMT</pubDate>
    <dc:creator>pambrose</dc:creator>
    <dc:date>2026-02-03T21:53:41Z</dc:date>
    <item>
      <title>MPXV7002 Reference Pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262369#M6519</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a quick question regarding the single port variants of the&amp;nbsp;MPXV7002 pressure sensors. I just wanted to confirm that these single port models are referencing port 1 pressure to the sensor's ambient pressure, and not an internal vacuum. It seems that the latter would exceed the device's maximum pressure rating of 75 kPa, but I just wanted to make sure. Thank you,&lt;/P&gt;&lt;P&gt;Austin&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262369#M6519</guid>
      <dc:creator>pambrose</dc:creator>
      <dc:date>2026-02-03T21:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV7002 Reference Pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262452#M6520</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The single ported versions of the MPXV7002 are all Gauge Pressure sensors, which means that the reference pressure is open to local atmospheric pressure.&lt;/P&gt;
&lt;P&gt;The reference pressure ‘port’ on Gauge sensors is an open hole in the bottom of the sensor, while port ‘P1’ is the one used to attach to the hose to measure the pressure.&lt;/P&gt;
&lt;P&gt;You need to make sure that the differential pressure between port P1 and reference pressure is never higher than 75kPa.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jose&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 03:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262452#M6520</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2021-04-15T03:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV7002 Reference Pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262474#M6521</link>
      <description>&lt;P&gt;Hi Reyes,&lt;/P&gt;&lt;P&gt;Perfect. Than you for clarifying and for your quick reply. Cheers,&lt;/P&gt;&lt;P&gt;Austin&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 04:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV7002-Reference-Pressure/m-p/1262474#M6521</guid>
      <dc:creator>pambrose</dc:creator>
      <dc:date>2021-04-15T04:38:55Z</dc:date>
    </item>
  </channel>
</rss>