<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Consecutive Reads in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Consecutive-Reads/m-p/293410#M651</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the MPL115A2 over the I2C bus. I need to know if the device supports consecutive read. I.e. If I write the address pointer to 0x00 and send a read command with 4 bytes worth of clock cycles( 4 x 9 clock pulses on the SCL line), will it send me pressure MSB, LSB, temperature MSB, and LSB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Onkar Raut,&lt;/P&gt;&lt;P&gt;Embedded Systems Engineer,&lt;/P&gt;&lt;P&gt;BNS Solutions, Walpole, MA.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:25:29 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2026-02-03T21:25:29Z</dc:date>
    <item>
      <title>Consecutive Reads</title>
      <link>https://community.nxp.com/t5/Sensors/Consecutive-Reads/m-p/293410#M651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the MPL115A2 over the I2C bus. I need to know if the device supports consecutive read. I.e. If I write the address pointer to 0x00 and send a read command with 4 bytes worth of clock cycles( 4 x 9 clock pulses on the SCL line), will it send me pressure MSB, LSB, temperature MSB, and LSB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Onkar Raut,&lt;/P&gt;&lt;P&gt;Embedded Systems Engineer,&lt;/P&gt;&lt;P&gt;BNS Solutions, Walpole, MA.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:25:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Consecutive-Reads/m-p/293410#M651</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2026-02-03T21:25:29Z</dc:date>
    </item>
    <item>
      <title>Re: Consecutive Reads</title>
      <link>https://community.nxp.com/t5/Sensors/Consecutive-Reads/m-p/293411#M652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Onkar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it will. The MPL115A2 does support a multiple-byte (burst) read.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2013 10:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Consecutive-Reads/m-p/293411#M652</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2013-11-25T10:17:31Z</dc:date>
    </item>
  </channel>
</rss>