<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: powering FXTH870xD sensor</title>
    <link>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1248722#M6491</link>
    <description>&lt;P&gt;Hi Victor,&lt;/P&gt;
&lt;P&gt;The choice of the battery has to be made taking into account several parameters like capacity, maximum current peak supported and temperature operating range.&lt;/P&gt;
&lt;P&gt;Regarding the capacity, it is common in TPMS applications to use a 120mAh battery and achieve 10 years of battery life. It depends on the wakeup period i.e. the period at which the measurements and RF transmissions are performed.&lt;/P&gt;
&lt;P&gt;If you create a standard &lt;A href="https://support.nxp.com/" target="_self"&gt;ticket&lt;/A&gt;, I can share with you an Excel file that helps to estimate the power consumption.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
    <pubDate>Fri, 19 Mar 2021 08:06:34 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2021-03-19T08:06:34Z</dc:date>
    <item>
      <title>powering FXTH870xD sensor</title>
      <link>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1241642#M6490</link>
      <description>&lt;P&gt;what the best solution to power&amp;nbsp;FXTH870xD sensor from battary?&lt;/P&gt;&lt;P&gt;is it possible to use CR2032 and get life &amp;gt; 1year ?&lt;/P&gt;&lt;P&gt;PS:&amp;nbsp;Sensor used without RF transmitter.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1241642#M6490</guid>
      <dc:creator>VictorOsipov</dc:creator>
      <dc:date>2026-02-03T20:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: powering FXTH870xD sensor</title>
      <link>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1248722#M6491</link>
      <description>&lt;P&gt;Hi Victor,&lt;/P&gt;
&lt;P&gt;The choice of the battery has to be made taking into account several parameters like capacity, maximum current peak supported and temperature operating range.&lt;/P&gt;
&lt;P&gt;Regarding the capacity, it is common in TPMS applications to use a 120mAh battery and achieve 10 years of battery life. It depends on the wakeup period i.e. the period at which the measurements and RF transmissions are performed.&lt;/P&gt;
&lt;P&gt;If you create a standard &lt;A href="https://support.nxp.com/" target="_self"&gt;ticket&lt;/A&gt;, I can share with you an Excel file that helps to estimate the power consumption.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 08:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1248722#M6491</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-03-19T08:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: powering FXTH870xD sensor</title>
      <link>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1249367#M6499</link>
      <description>&lt;P&gt;case&amp;nbsp;&lt;SPAN&gt;00****84 created, if it is possible - please answer in suitable time with attached document...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 06:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/powering-FXTH870xD-sensor/m-p/1249367#M6499</guid>
      <dc:creator>VictorOsipov</dc:creator>
      <dc:date>2021-03-22T06:21:26Z</dc:date>
    </item>
  </channel>
</rss>