<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックNXP5100AP</title>
    <link>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159277#M6295</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using NXP5100AP sensor for measurement barometric pressure. And have some trouble with precision.&lt;/P&gt;&lt;P&gt;In documentation is maximum error 2.5%. And in transfer function is error defined as &lt;SPAN&gt;± (Pressure Error x Temp. Mult. x 0.009 x V&lt;/SPAN&gt;&lt;SPAN&gt;S&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;Means this that 2.5% error is manufacturing calibration error? And error in transfer function is measurement error?&lt;/P&gt;&lt;P&gt;Question is if the 2.5% error is stable and if I can calibrate this error in MCU?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Fri, 25 Sep 2020 10:22:02 GMT</pubDate>
    <dc:creator>karloss</dc:creator>
    <dc:date>2020-09-25T10:22:02Z</dc:date>
    <item>
      <title>NXP5100AP</title>
      <link>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159277#M6295</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using NXP5100AP sensor for measurement barometric pressure. And have some trouble with precision.&lt;/P&gt;&lt;P&gt;In documentation is maximum error 2.5%. And in transfer function is error defined as &lt;SPAN&gt;± (Pressure Error x Temp. Mult. x 0.009 x V&lt;/SPAN&gt;&lt;SPAN&gt;S&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;Means this that 2.5% error is manufacturing calibration error? And error in transfer function is measurement error?&lt;/P&gt;&lt;P&gt;Question is if the 2.5% error is stable and if I can calibrate this error in MCU?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 10:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159277#M6295</guid>
      <dc:creator>karloss</dc:creator>
      <dc:date>2020-09-25T10:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: NXP5100AP</title>
      <link>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159333#M6296</link>
      <description>&lt;P&gt;Hello Karloss,&lt;/P&gt;
&lt;P&gt;your conclusion is correct.&amp;nbsp;&lt;SPAN&gt;The MPX5100GP is factory calibrated and temperature compensated, after this calibration, it is normal to have variation on the output for the pressure sensors, according to the datasheet should be ~+/-2.5%.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;You can do the calibration with your MCU. It is even recommended to implement Auto-zero calibration in our pressure sensors, this is a compensation technique based on sampling the offset of the sensor at reference pressure (atmospheric pressure is a zero reference for a gauge measurement) in order to correct the sensor output for long term offset drift or variation.&lt;BR /&gt;Please take a look at the Application Note AN1636 on the following link for the instructions for implement this technique.&lt;BR /&gt;AN1636: &lt;A href="https://www.nxp.com/docs/en/application-note/AN1636.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1636.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please note, that the device is ratiometric, which means, that the output varies with the change in supply voltage. Therefore a stable 5V supply voltage is recommended&amp;nbsp;&lt;SPAN&gt;and use one 1.0uF and one 0.01uF decoupling capacitors placed close to Vs pin of the pressure sensor, and a 470pF capacitor close to the Vout pin as an output filter capacitor.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 12:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159333#M6296</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2020-09-25T12:13:57Z</dc:date>
    </item>
    <item>
      <title>Re: NXP5100AP</title>
      <link>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159343#M6297</link>
      <description>&lt;P&gt;Thank you for information. I will to try MCU calibration. I think that Auto-zero is not usable in this case because I measuring atmospheric pressure....&lt;/P&gt;&lt;P&gt;The second option is use some sensor with better precision MPX4115AP looks better but is not easy available in CZ....&lt;/P&gt;&lt;P&gt;Karel&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 12:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159343#M6297</guid>
      <dc:creator>karloss</dc:creator>
      <dc:date>2020-09-25T12:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: NXP5100AP</title>
      <link>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159675#M6298</link>
      <description>&lt;P&gt;&amp;nbsp;Hello Karloss,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can do the Auto-Zero calibration for the MPX5100AP. It has its own internal reference. The quote "(atmospheric pressure is a zero reference for a gauge measurement)" is meant, that the MPX5100GP or GC6U or GC7U has not internal reference, but the atmospheric pressure should be taken as a reference.&lt;/P&gt;
&lt;P&gt;Yes for the moment, there is a shortage of pressure sensors due to significant unforecasted Covid19 medical demand for respirators/ventilators.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2020 06:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP5100AP/m-p/1159675#M6298</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2020-09-27T06:53:03Z</dc:date>
    </item>
  </channel>
</rss>