<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 fxls8962af</title>
    <link>https://community.nxp.com/t5/Sensors/fxls8962af/m-p/1153535#M6289</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Working on FXLS8962AF Accelerometer ic interfacing with 16 bit micro xc2321 infineon.&lt;/P&gt;&lt;P&gt;This sensor works on 24 clock pulses . able to transfer data in first 16 pulses . unable to transfer data in the last 8 bits .&lt;/P&gt;&lt;P&gt;Can any one support ?&lt;/P&gt;&lt;P&gt;This IC is connected in&amp;nbsp;SPI (4 Wire) &amp;nbsp;Mode . Can any one share the code with register settings .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:59:09 GMT</pubDate>
    <dc:creator>SRI2</dc:creator>
    <dc:date>2026-02-03T21:59:09Z</dc:date>
    <item>
      <title>fxls8962af</title>
      <link>https://community.nxp.com/t5/Sensors/fxls8962af/m-p/1153535#M6289</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Working on FXLS8962AF Accelerometer ic interfacing with 16 bit micro xc2321 infineon.&lt;/P&gt;&lt;P&gt;This sensor works on 24 clock pulses . able to transfer data in first 16 pulses . unable to transfer data in the last 8 bits .&lt;/P&gt;&lt;P&gt;Can any one support ?&lt;/P&gt;&lt;P&gt;This IC is connected in&amp;nbsp;SPI (4 Wire) &amp;nbsp;Mode . Can any one share the code with register settings .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/fxls8962af/m-p/1153535#M6289</guid>
      <dc:creator>SRI2</dc:creator>
      <dc:date>2026-02-03T21:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: fxls8962af</title>
      <link>https://community.nxp.com/t5/Sensors/fxls8962af/m-p/1153960#M6291</link>
      <description>&lt;P&gt;Hi Sriram,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately, I am not familiar with this Infineon’s MCU, but you are correct that both single byte read and write SPI transactions are completed in 24 clock pulses.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, you need to make sure there is no CS transition between the first 16 bits and the following 8 data bits. Your chip select output will have to be driven manually as a GPO.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, if your SPI module only allows to send x * 16 bits of data, you will have to likely implement software SPI using GPIOs to make sure you send out 24 and not 32 bits.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As for the example code, I will send it to you through your case #00306939.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 07:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/fxls8962af/m-p/1153960#M6291</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-09-16T07:41:28Z</dc:date>
    </item>
  </channel>
</rss>