<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ultra low power accelerometer in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288073#M627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dieter&lt;/P&gt;&lt;P&gt;Yes, I think you can use &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL1x"&gt;KL15&lt;/A&gt; and analog sensor for your application. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Apr 2013 11:36:45 GMT</pubDate>
    <dc:creator>Paul_Tian</dc:creator>
    <dc:date>2013-04-29T11:36:45Z</dc:date>
    <item>
      <title>Ultra low power accelerometer</title>
      <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288070#M624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL05Z" target="_blank"&gt;FRDM-KL05Z&lt;/A&gt; board comes with a built in MMA8451Q accelerometer with I2C interface. In general I2C isn't the best idea for ultra low power demo, because it is so slow. We need to run the processor at least 100 to 200 usec to get the accelerometer readout (6 Bytes + overhead).&lt;/P&gt;&lt;P&gt;Then i connected a LIS331HH SPI/I2C accelerometer and implemented SPI at 24 MHz/4 to get the readout within 12 usec, which is a lot better. I can get this down to about 8 usec with 20 MHz/2. But the SPI accelerometer has much more noise (650 versus 130 or 100 ug/sqrt(Hz)). This means the onboard accelerometer of the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL05Z" target="_blank"&gt;FRDM-KL05Z&lt;/A&gt; is a lot better concerning noise.&lt;/P&gt;&lt;P&gt;Is this because it is I2C? Can we use the MMA8451Q with SPI? Is there/will there be a SPI version of the MMA8451Q that serves better for ultra low power applications?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288070#M624</guid>
      <dc:creator>dieterteuchert</dc:creator>
      <dc:date>2026-02-03T21:09:03Z</dc:date>
    </item>
    <item>
      <title>Re: Ultra low power accelerometer</title>
      <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288071#M625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dieter&lt;/P&gt;&lt;P&gt;The I2C interface in &lt;A href="http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=KINETIS_L_SERIES"&gt;KL series&lt;/A&gt; is designed to operate up to 400 kbit/s with maximum bus loading and timing. The I2C device is capable of operating at higher baud rates, up to a maximum of clock/20, with reduced bus loading.&lt;/P&gt;&lt;P&gt;I find a g-sensor with SPI interface for your reference. Please check if MMA745xL series meet your requirement. You can find some material from link.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMA745xL&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMA745xL&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Hope my reply can help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Paul&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Apr 2013 01:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288071#M625</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-04-28T01:35:51Z</dc:date>
    </item>
    <item>
      <title>Re: Ultra low power accelerometer</title>
      <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288072#M626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response. I could not find a noise spec of the MMA745xL. It has a consumption of 400 uA and 10 bits of resolution.&lt;/P&gt;&lt;P&gt;As far as i understand, with a &lt;A href="http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=KINETIS_L_SERIES"&gt;Kinetis KL&lt;/A&gt; device onboard i can as well try an analog accelerometer. For example with a LIS344ALH, at 50 Hz x 2 msec usage, the current consumption could be as low as 70 uA plus the consumption of 150 ADC conversions per second in the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL1x"&gt;KL15&lt;/A&gt;. I mean from the low power point of view the analog transfer of acceleration measurements could be the best solution.&lt;/P&gt;&lt;P&gt;And the LIS344ALH has a noise spec of 50 ug/sqrt(Hz), which is even better than the MMA8451Q.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 09:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288072#M626</guid>
      <dc:creator>dieterteuchert</dc:creator>
      <dc:date>2013-04-29T09:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Ultra low power accelerometer</title>
      <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288073#M627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dieter&lt;/P&gt;&lt;P&gt;Yes, I think you can use &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL1x"&gt;KL15&lt;/A&gt; and analog sensor for your application. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 11:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288073#M627</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-04-29T11:36:45Z</dc:date>
    </item>
    <item>
      <title>Re: Ultra low power accelerometer</title>
      <link>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288074#M628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dieter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regarding your last question, we are planning to launch such a part in June with full production. It will be basically the same device as the MMA8451Q, but now including the SPI. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Have you considered using the embedded FIFO buffer on the MMA8451Q? It is very useful for system power savings and minimizing traffic across the I2C bus. Look at our &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4073.pdf"&gt;AN4073&lt;/A&gt; for more information on the embedded FIFO buffer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 12:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Ultra-low-power-accelerometer/m-p/288074#M628</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2013-04-29T12:32:12Z</dc:date>
    </item>
  </channel>
</rss>