<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMMA8453 Transient detection</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8453-Transient-detection/m-p/286914#M620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In regards to reading the actual acceleration data of an MMA8453, would I need to take into consideration the reference gravitational force?&amp;nbsp; For example, in reference to Figure 3 in the MMA8453Q datasheet, the "SIDE, FRONT" view shows 1g in the Z direction. If the device is set for a transient detection value of 2g, would the device be triggered at a Z force of 2g, or 3g, since there is already a 1g force, due to gravity? Will the data in the Zout register read the actual value of the force, or will the data be compensated for according to the 1g reference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your advice,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:04:17 GMT</pubDate>
    <dc:creator>georgek</dc:creator>
    <dc:date>2026-02-03T23:04:17Z</dc:date>
    <item>
      <title>MMA8453 Transient detection</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8453-Transient-detection/m-p/286914#M620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In regards to reading the actual acceleration data of an MMA8453, would I need to take into consideration the reference gravitational force?&amp;nbsp; For example, in reference to Figure 3 in the MMA8453Q datasheet, the "SIDE, FRONT" view shows 1g in the Z direction. If the device is set for a transient detection value of 2g, would the device be triggered at a Z force of 2g, or 3g, since there is already a 1g force, due to gravity? Will the data in the Zout register read the actual value of the force, or will the data be compensated for according to the 1g reference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your advice,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8453-Transient-detection/m-p/286914#M620</guid>
      <dc:creator>georgek</dc:creator>
      <dc:date>2026-02-03T23:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8453 Transient detection</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8453-Transient-detection/m-p/286915#M621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi George,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;The embedded transient detection function uses the high-pass filtered data unless the HPF_BYP bit in the TRANSIENT_CFG register (0x1D) is set. So if HPF_BYP = 0, the transient detection function compares whether any of the enabled axes has exceeded a set change in acceleration disregarding the static acceleration. Please refer to the &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4071.pdf"&gt;AN4071&lt;/A&gt; for more information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;However, compared with both the MMA8451Q and MMA8452Q, the MMA8453Q does not allow to set the high-pass filter for the output data using the HPF_OUT bit in the XYZ_DATA_CFG register (0x0E), so the data registers 0x01 - 0x06 will not contain high-pass filtered data.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;I hope it helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 13:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8453-Transient-detection/m-p/286915#M621</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2014-01-06T13:03:56Z</dc:date>
    </item>
  </channel>
</rss>