<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how to use MMA8653FC to implement tilt protection  in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041359#M6115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hardy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The easiest way to implement it is to use an embedded orientation detection function where you can set the threshold angle to 30° and enable the orientation function interrupt to notify/wake-up your MCU when this threshold is crossed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108112i775B4CEEE5DC057F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can be done using the MMA8652FC only, the MMA8653FC has a fixed threshold angle at 45°. For more information on the embedded orientation detection function please refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4068.pdf"&gt;AN4068&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another option is to periodically read and&amp;nbsp;analyze the acceleration data by your MCU. 30° corresponds to 0.5g or 0x80 (@ 10-bit data and ±2g mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should be no conflicts between these two interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Apr 2020 10:57:28 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2020-04-16T10:57:28Z</dc:date>
    <item>
      <title>how to use MMA8653FC to implement tilt protection</title>
      <link>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041358#M6114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have an application of compressor fridge on the vehicle, there should be a tilt protection function for the compressor. for example, if the angle is more 30 degree vs horizontal direction, to switch off compressor.&lt;/P&gt;&lt;P&gt;I want to know how to use MMA8653FC to implement this tilt protection function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;another question : the fridge unit is as a LIN slave node on the system, is there any conflicts between LIN communication and I2C communication, or is I2C communication interruptible by LIN communication interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041358#M6114</guid>
      <dc:creator>hardy_xiang</dc:creator>
      <dc:date>2026-02-03T21:52:30Z</dc:date>
    </item>
    <item>
      <title>Re: how to use MMA8653FC to implement tilt protection</title>
      <link>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041359#M6115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hardy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The easiest way to implement it is to use an embedded orientation detection function where you can set the threshold angle to 30° and enable the orientation function interrupt to notify/wake-up your MCU when this threshold is crossed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108112i775B4CEEE5DC057F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can be done using the MMA8652FC only, the MMA8653FC has a fixed threshold angle at 45°. For more information on the embedded orientation detection function please refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4068.pdf"&gt;AN4068&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another option is to periodically read and&amp;nbsp;analyze the acceleration data by your MCU. 30° corresponds to 0.5g or 0x80 (@ 10-bit data and ±2g mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should be no conflicts between these two interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2020 10:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041359#M6115</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-04-16T10:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: how to use MMA8653FC to implement tilt protection</title>
      <link>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041360#M6116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your quick answer,It is a helpful guidance for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;hardy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 00:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/how-to-use-MMA8653FC-to-implement-tilt-protection/m-p/1041360#M6116</guid>
      <dc:creator>hardy_xiang</dc:creator>
      <dc:date>2020-04-17T00:56:06Z</dc:date>
    </item>
  </channel>
</rss>