<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MPR proximity range max distance</title>
    <link>https://community.nxp.com/t5/Sensors/MPR-proximity-range-max-distance/m-p/284301#M603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can increase the distance by increasing the charge/discharge current and more importantly, increasing the size of the electrode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Steffen&lt;/P&gt;&lt;P&gt;Senior Field Applications Engineer&lt;/P&gt;&lt;P&gt;Freescale Semiconductor&lt;/P&gt;&lt;P&gt;Cell 815-519-1567&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2014 19:23:12 GMT</pubDate>
    <dc:creator>michaelsteffenf</dc:creator>
    <dc:date>2014-02-07T19:23:12Z</dc:date>
    <item>
      <title>MPR proximity range max distance</title>
      <link>https://community.nxp.com/t5/Sensors/MPR-proximity-range-max-distance/m-p/284300#M602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-top: auto; margin-bottom: 12.0pt;"&gt;I was experimenting with the MPR121 for proximity, and have managed to get a basic demo up and running. I am getting the distance as 2-3 cm, is there anyway we can increase the distance?&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: 12.0pt;"&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Some suggestions with the register values might help, as well as suggestions for electrode material ? I am currently using aluminium foil as a test.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: 12.0pt;"&gt;The current configuration of the registers I am using is :&lt;BR /&gt; &lt;BR /&gt; // prox sensing rising&lt;BR /&gt; MaxHalfDeltaRising, 0x3F&lt;BR /&gt; NoiseHalfDeltaAmountR, 0x5F&lt;BR /&gt; NoiseCountLimitRising, 0x04&lt;BR /&gt; FilterDelayLimitR, 0x00);&lt;BR /&gt; &lt;BR /&gt; // prox sensing falling&lt;BR /&gt; MHDF, 0x01&lt;BR /&gt; NHDAF, 0x01&lt;BR /&gt; NCLF, 0x1F&lt;BR /&gt; NDLF, 0x04&lt;BR /&gt; &lt;BR /&gt; // Section D - Set the touch filter Configuration&lt;BR /&gt; FIL_CFG, 0x24&lt;BR /&gt; &lt;BR /&gt;I have disabled auto config and auto reconfig, but here were the original settings&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN style="font-size: 12.0pt; font-family: 'Times New Roman','serif';"&gt;ElectrodeConfig, 0x30&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 13:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR-proximity-range-max-distance/m-p/284300#M602</guid>
      <dc:creator>manaschhabra-b1</dc:creator>
      <dc:date>2014-02-07T13:55:11Z</dc:date>
    </item>
    <item>
      <title>Re: MPR proximity range max distance</title>
      <link>https://community.nxp.com/t5/Sensors/MPR-proximity-range-max-distance/m-p/284301#M603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can increase the distance by increasing the charge/discharge current and more importantly, increasing the size of the electrode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Steffen&lt;/P&gt;&lt;P&gt;Senior Field Applications Engineer&lt;/P&gt;&lt;P&gt;Freescale Semiconductor&lt;/P&gt;&lt;P&gt;Cell 815-519-1567&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 19:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR-proximity-range-max-distance/m-p/284301#M603</guid>
      <dc:creator>michaelsteffenf</dc:creator>
      <dc:date>2014-02-07T19:23:12Z</dc:date>
    </item>
  </channel>
</rss>