<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mpx5500 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/mpx5500/m-p/284137#M601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPX5500 is an integrated pressure sensor which means that the sensor is already Temperature Compensated, Calibrated and amplified internally, so the output of the sensor will be from 0 to 5.0V depending on the pressure applied.&lt;/P&gt;&lt;P&gt;The hardware needed to connect it to a MCU is minimal, you can find the recommended connection on Figure 4 of the datasheet: &lt;A href="http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf" title="http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf"&gt;http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Mar 2014 22:34:32 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2014-03-10T22:34:32Z</dc:date>
    <item>
      <title>mpx5500</title>
      <link>https://community.nxp.com/t5/Sensors/mpx5500/m-p/284136#M600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I need to connect MPX5500 to PIC18F MCU so MCU has itself comparator or I can use separate op amp &lt;/P&gt;&lt;P&gt;What is the most suitable way to connect MPX5500 to MCU &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Please help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/mpx5500/m-p/284136#M600</guid>
      <dc:creator>PA3040</dc:creator>
      <dc:date>2026-02-03T23:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: mpx5500</title>
      <link>https://community.nxp.com/t5/Sensors/mpx5500/m-p/284137#M601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPX5500 is an integrated pressure sensor which means that the sensor is already Temperature Compensated, Calibrated and amplified internally, so the output of the sensor will be from 0 to 5.0V depending on the pressure applied.&lt;/P&gt;&lt;P&gt;The hardware needed to connect it to a MCU is minimal, you can find the recommended connection on Figure 4 of the datasheet: &lt;A href="http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf" title="http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf"&gt;http://cache.freescale.com/files/sensors/doc/data_sheet/MPX5500.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Mar 2014 22:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/mpx5500/m-p/284137#M601</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2014-03-10T22:34:32Z</dc:date>
    </item>
  </channel>
</rss>