<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPR121 Proximity Detection in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPR121-Proximity-Detection/m-p/979281#M5935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. First of all, If the panel grows, the noise will also grow. And if the integrated power of a panel of that size is not enough.&lt;BR /&gt;Assuming that these two problems do not exist, for the filter;&lt;BR /&gt;Use the bubble sort method inside the Arduino program. It really works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 08:00:57 GMT</pubDate>
    <dc:creator>recep</dc:creator>
    <dc:date>2020-03-18T08:00:57Z</dc:date>
    <item>
      <title>MPR121 Proximity Detection</title>
      <link>https://community.nxp.com/t5/Sensors/MPR121-Proximity-Detection/m-p/979280#M5934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm new here in the forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With&amp;nbsp;Arduino I'm trying to get the proximity work on a large conductivity panel (about 1meters x 2meters) using a MPR121 equipped board:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://wiki.seeedstudio.com/Grove-12_Key_Capacitive_I2C_Touch_Sensor_V2-MPR121/" title="http://wiki.seeedstudio.com/Grove-12_Key_Capacitive_I2C_Touch_Sensor_V2-MPR121/"&gt;Grove - 12 Key Capacitive I2C Touch Sensor V2(MPR121) - Seeed Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following this application note &lt;A href="https://cache.freescale.com/files/sensors/doc/app_note/AN3893.pdf"&gt;A3893&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;I set the register for area detection (0x5E) and I read the baseline and datas from registers (0x1C, 0x1B, 0x2A).&lt;/P&gt;&lt;P&gt;But I'm not able to get stable data from the 13th pseudo electrode, the values are very&amp;nbsp;fluctuating and inconsistent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where I'm wrong? There are another register settings to do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 17:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR121-Proximity-Detection/m-p/979280#M5934</guid>
      <dc:creator>andreabruno</dc:creator>
      <dc:date>2019-11-12T17:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPR121 Proximity Detection</title>
      <link>https://community.nxp.com/t5/Sensors/MPR121-Proximity-Detection/m-p/979281#M5935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. First of all, If the panel grows, the noise will also grow. And if the integrated power of a panel of that size is not enough.&lt;BR /&gt;Assuming that these two problems do not exist, for the filter;&lt;BR /&gt;Use the bubble sort method inside the Arduino program. It really works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 08:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR121-Proximity-Detection/m-p/979281#M5935</guid>
      <dc:creator>recep</dc:creator>
      <dc:date>2020-03-18T08:00:57Z</dc:date>
    </item>
  </channel>
</rss>