<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TPMS over-the-air software update. in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976419#M5926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Tomas,&lt;/P&gt;&lt;P&gt;In your description with replace the KW01 and LF antenna board with their own tools.&lt;/P&gt;&lt;P&gt;1. I am curious about if possible to replace the LF antenna board with HTRC110-based design? if yes, can I have the reference design?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. in the KW01+LF antenna board, it seems that MCU’s GPIO needs PWM wave generator for 125khz waveform? is that right?&lt;/P&gt;&lt;P&gt;and the SW need to control timing of the each bit time after convert the data bit to manchester code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;thanks for giving me guidance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 14:46:55 GMT</pubDate>
    <dc:creator>anthonyhhfu</dc:creator>
    <dc:date>2020-06-10T14:46:55Z</dc:date>
    <item>
      <title>TPMS over-the-air software update.</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976417#M5924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I'm working on a TPMS project,&amp;nbsp;The chip used is FXTH87E.&amp;nbsp;I'm debugging the wireless software upgrade,&amp;nbsp;I downloaded embedded software in FXTH87E location, LF/RF BootLoader.&amp;nbsp;I didn't understand the application manual, and I felt that the steps of the project explanation were not detailed enough.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Must the active controller use Kinetis MKW01Z128 MCU?&amp;nbsp;I now have a TPMS maintenance detection device that can send a low-frequency signal of 125k. However, I used CW11.1 to burn TPMS_BtLdr_1 on FXTH87E for debugging, and found no reaction in the debugging interface.&amp;nbsp;Can FXTH87E be activated by 125k low frequency signal?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;How to activate FXTH87E with 125k low frequency signal?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;One more question,&amp;nbsp;What is the role of cu8BootEntryKey in the TPMS_BtLdr_1 project code?&amp;nbsp;Is this key required between the device sending low frequency signal and FXTH87E receiving low frequency signal?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976417#M5924</guid>
      <dc:creator>guwenlong_l</dc:creator>
      <dc:date>2026-02-03T21:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS over-the-air software update.</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976418#M5925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find below the answers from our TPMS software engineer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;Figure 7 of the Application Note gives a system overview: the TPMS receives LF commands and send RF commands. In our demo, to transmit LF frames and receive RF frames we are using a KW01 board connected to a LF antenna board. The MKW01 software and TPMS software have been developed to work together, they are compatible with each other in terms of LF and RF frame format, timing etc…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a final application, users will replace the KW01 + LF antenna with their own tools, and will have to update the TPMS software to be compatible with their tool, in terms of frame format, timing etc…&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98071i126FBEA443653BCD/image-size/large?v=v2&amp;amp;px=999" title="Fig 7.jpg" alt="Fig 7.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;All frame formats are described in the document 2018-01-23_BtLdr_Comm_Packets provided in the package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;If the LF frame received contains this data then the TPMS enters Bootloader State 1. The transition flow is described in Figure 3 of the Application Note.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98142i0297B5BE2635CB70/image-size/large?v=v2&amp;amp;px=999" title="Pic 2.jpg" alt="Pic 2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it fully clarifies your questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 08:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976418#M5925</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-03-18T08:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS over-the-air software update.</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976419#M5926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Tomas,&lt;/P&gt;&lt;P&gt;In your description with replace the KW01 and LF antenna board with their own tools.&lt;/P&gt;&lt;P&gt;1. I am curious about if possible to replace the LF antenna board with HTRC110-based design? if yes, can I have the reference design?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. in the KW01+LF antenna board, it seems that MCU’s GPIO needs PWM wave generator for 125khz waveform? is that right?&lt;/P&gt;&lt;P&gt;and the SW need to control timing of the each bit time after convert the data bit to manchester code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;thanks for giving me guidance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 14:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-over-the-air-software-update/m-p/976419#M5926</guid>
      <dc:creator>anthonyhhfu</dc:creator>
      <dc:date>2020-06-10T14:46:55Z</dc:date>
    </item>
  </channel>
</rss>