<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 vacuum pressure sensor</title>
    <link>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907803#M5722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for a vacuum pressure sensor to control a process that operates at -2kPa from ambient atmosphere.&lt;/P&gt;&lt;P&gt;The temperature operating range is from +10 to +50C.&lt;/P&gt;&lt;P&gt;I'm looking for accuracy equal or better than 5%.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:04:02 GMT</pubDate>
    <dc:creator>cram1</dc:creator>
    <dc:date>2026-02-03T22:04:02Z</dc:date>
    <item>
      <title>vacuum pressure sensor</title>
      <link>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907803#M5722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for a vacuum pressure sensor to control a process that operates at -2kPa from ambient atmosphere.&lt;/P&gt;&lt;P&gt;The temperature operating range is from +10 to +50C.&lt;/P&gt;&lt;P&gt;I'm looking for accuracy equal or better than 5%.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907803#M5722</guid>
      <dc:creator>cram1</dc:creator>
      <dc:date>2026-02-03T22:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: vacuum pressure sensor</title>
      <link>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907804#M5723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your application, the best sensor will be the:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-2-to-2kpa-vacuum-pressure-sensor:MPXV7002"&gt;MPXV7002&lt;/A&gt; Pressure range= -2 to 2kPa; temperature compensated over 10° to 60°C; 2.5% Typical Error over +10°C to +60°C with Auto Zero and 6.25% Maximum Error over +10°C to +60°C without Auto Zero.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just in case that you can be interested in a higher pressure range, please see below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-7-to-7kpa-differential-and-gauge-pressure-sensor:MPXV7007DP"&gt;MPXV7007DP&lt;/A&gt; Pressure range= -7 to 7kPa; Temperature Compensated Over –40° to +125°C and 5.0% Maximum Error Over 0° to 85°C.&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-25-to-25kpa-differential-and-gauge-pressure-sensor:MPXV7025DP"&gt;MPXV70025DP&lt;/A&gt; Pressure range= -25 to 25kPa; Temperature Compensated Over –40° to +125°C and 5.0% Maximum Error Over 0° to 85°C.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can be helpful.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 20:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907804#M5723</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2019-05-27T20:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: vacuum pressure sensor</title>
      <link>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907805#M5724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i will go with&amp;nbsp;MPXV7002, thanks a lot &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lisettelozano"&gt;lisettelozano&lt;/A&gt;‌&amp;nbsp;&lt;A ___default_attr="282782" _modifiedtitle="true" _title="Lisette Paulina Lozano Gomez" class="link-titled" data-orig-content="Lisette Paulina Lozano Gomez" href="https://mcdvoice.dev/" jivemacro="user" title="https://mcdvoice.dev/"&gt;mcdvoice&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2019 19:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/vacuum-pressure-sensor/m-p/907805#M5724</guid>
      <dc:creator>esehi123</dc:creator>
      <dc:date>2019-06-03T19:44:19Z</dc:date>
    </item>
  </channel>
</rss>