<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Example FXOS8700CQ Driver Code in Datasheet gives 0,0,256 for magnetometer x,y,z values in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Example-FXOS8700CQ-Driver-Code-in-Datasheet-gives-0-0-256-for/m-p/899111#M5661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The FXOS8700 is connected to Beaglebone Black via i2c.&amp;nbsp;&amp;nbsp;&amp;nbsp; The example code from the Datasheet is copied - print statements were added.&amp;nbsp;&amp;nbsp; The accelerometer data seems fine but the magnetometer data is consistently 0,0,256.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The magnetometer control register 2,&amp;nbsp; FXOS8700CQ_M_CTRL_REG2, is being set to 0x20 for a burst read but it does not seem to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure if this is being posted in the correct location....#&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:05:20 GMT</pubDate>
    <dc:creator>peter_macleod_t</dc:creator>
    <dc:date>2026-02-03T22:05:20Z</dc:date>
    <item>
      <title>Example FXOS8700CQ Driver Code in Datasheet gives 0,0,256 for magnetometer x,y,z values</title>
      <link>https://community.nxp.com/t5/Sensors/Example-FXOS8700CQ-Driver-Code-in-Datasheet-gives-0-0-256-for/m-p/899111#M5661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The FXOS8700 is connected to Beaglebone Black via i2c.&amp;nbsp;&amp;nbsp;&amp;nbsp; The example code from the Datasheet is copied - print statements were added.&amp;nbsp;&amp;nbsp; The accelerometer data seems fine but the magnetometer data is consistently 0,0,256.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The magnetometer control register 2,&amp;nbsp; FXOS8700CQ_M_CTRL_REG2, is being set to 0x20 for a burst read but it does not seem to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure if this is being posted in the correct location....#&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Example-FXOS8700CQ-Driver-Code-in-Datasheet-gives-0-0-256-for/m-p/899111#M5661</guid>
      <dc:creator>peter_macleod_t</dc:creator>
      <dc:date>2026-02-03T22:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: Example FXOS8700CQ Driver Code in Datasheet gives 0,0,256 for magnetometer x,y,z values</title>
      <link>https://community.nxp.com/t5/Sensors/Example-FXOS8700CQ-Driver-Code-in-Datasheet-gives-0-0-256-for/m-p/899112#M5662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First off, please double check if&amp;nbsp;m_hms[1:0] = 0b11 (hybrid mode).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I would recommend to check what is going on the bus using an oscilloscope or a logic analyzer. I have used a burst read in my &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-101073"&gt;example&lt;/A&gt;&amp;nbsp;without any problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 08:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Example-FXOS8700CQ-Driver-Code-in-Datasheet-gives-0-0-256-for/m-p/899112#M5662</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-04-18T08:01:27Z</dc:date>
    </item>
  </channel>
</rss>