<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MMA8452 sensivity in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883472#M5602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First please accept my apologies for the late response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MMA8452 is a 12-bit data resolution with a 1024 counts/g on 2g mode. A way to increase the resolution is by oversampling. One of the oversampling schemes of the data can be activated when MODS = 10 in register 0x2B which will improve the resolution of the output data only. The highest resolution is achieved at 1.56 Hz. However, this can increase power usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details are shown in section 6 of the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4075.pdf"&gt;AN4075&lt;/A&gt;. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jul 2019 15:38:55 GMT</pubDate>
    <dc:creator>lisettelozano</dc:creator>
    <dc:date>2019-07-12T15:38:55Z</dc:date>
    <item>
      <title>MMA8452 sensivity</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883471#M5601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;sorry if this is a cross post.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I asked two years ago support for the best configuration of this sensor to detect vehicle motion and you pointed me in the right direction with some application notes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But sometimes, if the vehicle start slowly or the ground is flat and regular, I detect the movement with a delay, 30 seconds or more and it’s too much.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will move to a new devices with higher sensitivity in a new project, but for the current projects I’m trying to understand if I can optimise the configuration and improve sensitivity.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px; font-size: 14px;"&gt;&amp;nbsp;I'm actually using this configuration. Is there anything I can do ?&lt;/P&gt;&lt;P style="color: #51626f; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px; font-size: 14px;"&gt;$2A, [$18] ' 0x2A: CTRL_REG1 system control 1 register, Set device in 100Hz ODR, Standby&lt;BR /&gt;$1D, [$1E] ' 0x1D: Transient_CFG register, enable latch, Enable XYZ&lt;BR /&gt;$1F, [$01] ' 0x1F: TRANSIENT_THS register, set threshold to 1 counts&lt;BR /&gt;$20, [$05] ' 0x20: TRANSIENT_COUNT, set debounce 50mS&lt;BR /&gt;$2D, [$20] ' 0x2D: CTRL_REG4 register, enable transient interrupt&lt;BR /&gt;$2E, [$20] ' 0x2E: CTRL_REG5 interrupt configuration register, Route the Transient Interrupt to INT 1 hardware pin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883471#M5601</guid>
      <dc:creator>marcick</dc:creator>
      <dc:date>2026-02-03T22:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8452 sensivity</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883472#M5602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First please accept my apologies for the late response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MMA8452 is a 12-bit data resolution with a 1024 counts/g on 2g mode. A way to increase the resolution is by oversampling. One of the oversampling schemes of the data can be activated when MODS = 10 in register 0x2B which will improve the resolution of the output data only. The highest resolution is achieved at 1.56 Hz. However, this can increase power usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details are shown in section 6 of the &lt;A href="https://www.nxp.com/docs/en/application-note/AN4075.pdf"&gt;AN4075&lt;/A&gt;. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2019 15:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883472#M5602</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2019-07-12T15:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8452 sensivity</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883473#M5603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Paulina,&lt;/P&gt;&lt;P&gt;I have moved to a 14 bit sensor for a new project but I'm still interested to this topic to improve performances of my previous 8452 based design.&lt;/P&gt;&lt;P&gt;So, thank you anyway for your late reply. I'll study that application note.&lt;/P&gt;&lt;P&gt;Greetings from Italy&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jul 2019 04:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8452-sensivity/m-p/883473#M5603</guid>
      <dc:creator>marcick</dc:creator>
      <dc:date>2019-07-13T04:56:22Z</dc:date>
    </item>
  </channel>
</rss>