<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Motion Detection MMA8451 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876615#M5543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning,&lt;/P&gt;&lt;P&gt;I've enabled the motion detection and now when my acceleration on the X-axis exceeds the threshold it works fine, but I want also that it continues to collect data while the device is moving at constant speed (acceleration = 0).&lt;/P&gt;&lt;P&gt;Does exist some embedded register to use the deceleration (breaking) as threshold for stop collecting data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for you time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luigi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:18:22 GMT</pubDate>
    <dc:creator>luigi5hd</dc:creator>
    <dc:date>2026-02-03T22:18:22Z</dc:date>
    <item>
      <title>Motion Detection MMA8451</title>
      <link>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876615#M5543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning,&lt;/P&gt;&lt;P&gt;I've enabled the motion detection and now when my acceleration on the X-axis exceeds the threshold it works fine, but I want also that it continues to collect data while the device is moving at constant speed (acceleration = 0).&lt;/P&gt;&lt;P&gt;Does exist some embedded register to use the deceleration (breaking) as threshold for stop collecting data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for you time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luigi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876615#M5543</guid>
      <dc:creator>luigi5hd</dc:creator>
      <dc:date>2026-02-03T22:18:22Z</dc:date>
    </item>
    <item>
      <title>Re: Motion Detection MMA8451</title>
      <link>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876616#M5544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luigi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The configurable threshold in the FF_MT_THS register is an absolute value and you can distinguish positive vs. negative using polarity flags (XHP, YHP and ZHP) in the FF_MT_SRC register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53712i5EEB65442D830F3D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51862iA17ACF34CCCA73A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 08:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876616#M5544</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-01-16T08:40:37Z</dc:date>
    </item>
    <item>
      <title>Re: Motion Detection MMA8451</title>
      <link>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876617#M5545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;Oh sure, you're right, I'd forgotten these register's proprieties.&lt;/P&gt;&lt;P&gt;But I have a question, the acceleration's polarity meanings are, for instance for the X axe:&lt;/P&gt;&lt;P&gt;if XHE = 1 we have an&amp;nbsp; acceleration&lt;/P&gt;&lt;P&gt;if XHP = 1 we have a braking (deceleration)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the polarity isn't correlated to the fact that I'm going forward or backward right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luigi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 14:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Motion-Detection-MMA8451/m-p/876617#M5545</guid>
      <dc:creator>luigi5hd</dc:creator>
      <dc:date>2019-01-16T14:32:18Z</dc:date>
    </item>
  </channel>
</rss>