<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMA8453 Detect false double tap in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8453-Detect-false-double-tap/m-p/856047#M5441</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMA8453 is placed inside a device which a person can carry while traveling. We've enabled double tap feature which the person can use in case of emergency. The problem is we're getting false double taps when the vehicle is moving.&lt;/P&gt;&lt;P&gt;Configuration:&lt;/P&gt;&lt;P&gt;REG_PULSE_CFG 0x2A&lt;/P&gt;&lt;P&gt;REG_PULSE_THSX 0x20&lt;/P&gt;&lt;P&gt;REG_PULSE_THSY 0x20&lt;/P&gt;&lt;P&gt;REG_PULSE_THSZ 0x40&lt;/P&gt;&lt;P&gt;REG_PULSE_TMLT 0x18&lt;/P&gt;&lt;P&gt;REG_PULSE_LTCY 0x28&lt;/P&gt;&lt;P&gt;REG_PULSE_WIND 0x3C&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prakash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:28:56 GMT</pubDate>
    <dc:creator>prakash1</dc:creator>
    <dc:date>2026-02-03T22:28:56Z</dc:date>
    <item>
      <title>MMA8453 Detect false double tap</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8453-Detect-false-double-tap/m-p/856047#M5441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMA8453 is placed inside a device which a person can carry while traveling. We've enabled double tap feature which the person can use in case of emergency. The problem is we're getting false double taps when the vehicle is moving.&lt;/P&gt;&lt;P&gt;Configuration:&lt;/P&gt;&lt;P&gt;REG_PULSE_CFG 0x2A&lt;/P&gt;&lt;P&gt;REG_PULSE_THSX 0x20&lt;/P&gt;&lt;P&gt;REG_PULSE_THSY 0x20&lt;/P&gt;&lt;P&gt;REG_PULSE_THSZ 0x40&lt;/P&gt;&lt;P&gt;REG_PULSE_TMLT 0x18&lt;/P&gt;&lt;P&gt;REG_PULSE_LTCY 0x28&lt;/P&gt;&lt;P&gt;REG_PULSE_WIND 0x3C&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prakash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8453-Detect-false-double-tap/m-p/856047#M5441</guid>
      <dc:creator>prakash1</dc:creator>
      <dc:date>2026-02-03T22:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8453 Detect false double tap</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8453-Detect-false-double-tap/m-p/856048#M5442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prakash,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have never heard of a similar problem and it is hard to provide any specific setting that would eliminate such unwanted triggers. My only recommendation is to adjust the threshold and duration values by testing it in a vehicle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 09:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8453-Detect-false-double-tap/m-p/856048#M5442</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-02-13T09:09:02Z</dc:date>
    </item>
  </channel>
</rss>