<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Differential Pressure Sensor Specifications in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Differential-Pressure-Sensor-Specifications/m-p/852161#M5385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, the MPXV5010DP (0 kPa to 10 kPa) will not be able to measure up to &amp;gt;70 kPa as per its maximum pressure range is 40 kPa (P1&amp;gt;P2); this value is specified in table 2 from the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The differential pressure specification refers to the measurement between two points where the pressure is applied to both sides (Port P1 and Port P2) of the sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to measure a pressure between 70 kPa and 80 kPa, we can recommend the MPXV5100DP (0 kPa to 100 kPa) differential pressure sensor. It has a maximum error of 2.5% over 0 to 85 °C. You can find more information here &lt;A href="https://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-115-kpa/0-to-100kpa-differential-gauge-and-absolute-integrated-pressure-sensor:MPX5100"&gt;https://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-115-kpa/0-to-100kpa-differential-gauge-and-absolute-integrated-pressure-sensor:MPX5100&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2019 23:05:12 GMT</pubDate>
    <dc:creator>lisettelozano</dc:creator>
    <dc:date>2019-01-24T23:05:12Z</dc:date>
    <item>
      <title>Differential Pressure Sensor Specifications</title>
      <link>https://community.nxp.com/t5/Sensors/Differential-Pressure-Sensor-Specifications/m-p/852160#M5384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using&amp;nbsp;a 0 - 10 kPa differential pressure sensor, can I measure 70 - 80&amp;nbsp;kPa pressure changes or would that require a 0 - 100 kPa sensor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've actually used a&amp;nbsp;MPXV5010DP (0 kPa to 10 kPa) sensor in this environment and it didn't work as well as I had hoped.&amp;nbsp; Wondering if it is the wrong sensor for the application.&amp;nbsp; Am I overpressurizing it?&amp;nbsp; I'm not sure if the differential pressure specification refers to a differential pressure "within" the specified range or if it means that it cancels out the differential pressure and is appropriate for a 10 kPa range. I actually need as much resolution as possible between 70 kPa and 71 kPa.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Differential-Pressure-Sensor-Specifications/m-p/852160#M5384</guid>
      <dc:creator>jeffreyswelch</dc:creator>
      <dc:date>2026-02-03T22:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: Differential Pressure Sensor Specifications</title>
      <link>https://community.nxp.com/t5/Sensors/Differential-Pressure-Sensor-Specifications/m-p/852161#M5385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, the MPXV5010DP (0 kPa to 10 kPa) will not be able to measure up to &amp;gt;70 kPa as per its maximum pressure range is 40 kPa (P1&amp;gt;P2); this value is specified in table 2 from the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The differential pressure specification refers to the measurement between two points where the pressure is applied to both sides (Port P1 and Port P2) of the sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to measure a pressure between 70 kPa and 80 kPa, we can recommend the MPXV5100DP (0 kPa to 100 kPa) differential pressure sensor. It has a maximum error of 2.5% over 0 to 85 °C. You can find more information here &lt;A href="https://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-115-kpa/0-to-100kpa-differential-gauge-and-absolute-integrated-pressure-sensor:MPX5100"&gt;https://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-115-kpa/0-to-100kpa-differential-gauge-and-absolute-integrated-pressure-sensor:MPX5100&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 23:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Differential-Pressure-Sensor-Specifications/m-p/852161#M5385</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2019-01-24T23:05:12Z</dc:date>
    </item>
  </channel>
</rss>