<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pressure Sensor Choiche in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-Choiche/m-p/851254#M5375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wold like to use a pressure sensor for fluidic application which can reach a maximum pressure of 1500kPascal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any advice? It should work also with liquid components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the FXTH87 usable with liquid?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mattia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:17:22 GMT</pubDate>
    <dc:creator>mattiad</dc:creator>
    <dc:date>2026-02-03T22:17:22Z</dc:date>
    <item>
      <title>Pressure Sensor Choiche</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-Choiche/m-p/851254#M5375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wold like to use a pressure sensor for fluidic application which can reach a maximum pressure of 1500kPascal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any advice? It should work also with liquid components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the FXTH87 usable with liquid?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mattia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-Choiche/m-p/851254#M5375</guid>
      <dc:creator>mattiad</dc:creator>
      <dc:date>2026-02-03T22:17:22Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor Choiche</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-Choiche/m-p/851255#M5376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mattia,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FXTH871xD is the only pressure sensor family in the current portfolio capable of measure pressure up to 1500 kPa.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For all NXP pressure sensor products, any environment other than dry air, will may have some impact on the reliability and lifetime of the product. NXP's silicon pressure sensors are NOT compatible with oil, gas, petrol and can be affected by water or water vapors, or other chemicals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;A determination must be made if this impact is acceptable for the application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 17:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-Choiche/m-p/851255#M5376</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-04-15T17:31:37Z</dc:date>
    </item>
  </channel>
</rss>