<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックFXTH87 STOP1 RTI Error</title>
    <link>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845632#M5344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using FXTH8711 with RTI to 32ms and PWU wake-up mode to 1 second. These 2 timers use LFO clock (always ON in RUN/STOPx modes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have one specific processus for RTI and one other for PWU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the PWU: the TPMS wake-up and resets from reset-vector and when in my application I enable INTERRUPT (CLI) it enters in PWU handler. It is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the RTI the TPMS stays in STOP1 mode and when it resets (PWU timeout reached) the RTI interrupt flag is not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is RTI timer running in STOP1 mode ? In the datasheet it is written that RTI timer can be used (with LFO clock) to wake-up from STOP1 because of interrupt event. It is indicated too that any reset (example: wake-up from STOP1 mode) clears the RTIF (RTI Flag pending event) so in my application I can never check if this timeout has been reached to execute a specific processus associated to RTI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me please ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Romain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:05:22 GMT</pubDate>
    <dc:creator>mhusthutchinson</dc:creator>
    <dc:date>2026-02-03T21:05:22Z</dc:date>
    <item>
      <title>FXTH87 STOP1 RTI Error</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845632#M5344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using FXTH8711 with RTI to 32ms and PWU wake-up mode to 1 second. These 2 timers use LFO clock (always ON in RUN/STOPx modes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have one specific processus for RTI and one other for PWU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the PWU: the TPMS wake-up and resets from reset-vector and when in my application I enable INTERRUPT (CLI) it enters in PWU handler. It is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the RTI the TPMS stays in STOP1 mode and when it resets (PWU timeout reached) the RTI interrupt flag is not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is RTI timer running in STOP1 mode ? In the datasheet it is written that RTI timer can be used (with LFO clock) to wake-up from STOP1 because of interrupt event. It is indicated too that any reset (example: wake-up from STOP1 mode) clears the RTIF (RTI Flag pending event) so in my application I can never check if this timeout has been reached to execute a specific processus associated to RTI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me please ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Romain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845632#M5344</guid>
      <dc:creator>mhusthutchinson</dc:creator>
      <dc:date>2026-02-03T21:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: FXTH87 STOP1 RTI Error</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845633#M5345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Romain,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Yes, the RTI can be used as wake-up source from STOP1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Below is an example of initialization to use the RTI as wake up source from STOP4 or STOP1:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // First clear flag&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SRTISC_RTIACK = SET;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Select LFO as clock&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SRTISC_RTICLKS = CLEAR;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SRTISC_RTIS = period; // where period takes one of the values specified in Table 24&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable interrupt // No effect for wake up from STOP1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SRTISC_RTIE = SET;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67894iA9483DF5AD47A23A/image-size/large?v=v2&amp;amp;px=999" title="Table 24.jpg" alt="Table 24.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;It is correct that upon wake up from STOP1 on RTI interrupt, there will be no associated flag in TPMS_INTERRUPT_FLAG or SIMSES register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;This fact can be used to determine if the wake up from STOP1 was due to RTI or not; for example the following can be done upon wake up from STOP1: if SPMSC2_PDF is set, TPMS_INTERRUPT_FLAG and SIMSES are clear and RTI interrupt was enabled before entering STOP1 (this information can be stored in a variable in the PARAM section) then the wake up was due to RTI and the specific process can be executed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Sep 2018 10:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845633#M5345</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-09-03T10:12:15Z</dc:date>
    </item>
    <item>
      <title>Re: FXTH87 STOP1 RTI Error</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845634#M5346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Romain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Sep 2018 12:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-STOP1-RTI-Error/m-p/845634#M5346</guid>
      <dc:creator>mhusthutchinson</dc:creator>
      <dc:date>2018-09-03T12:18:31Z</dc:date>
    </item>
  </channel>
</rss>