<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 6D Sensor Fusion Algorithm Problem</title>
    <link>https://community.nxp.com/t5/Sensors/6D-Sensor-Fusion-Algorithm-Problem/m-p/836106#M5308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some tests&amp;nbsp;with NXP Sensor Fusion Library on my custom hardware.&amp;nbsp;The library works pretty well under most conditions. But when I move the board forward and backward in less than 1 sec - periodically to test the behaviour under vibration (especially the board in a diagonal position to the surface), sometimes I see abrupt changes at output. Please find attached the pictures. In the pictures, the blue line is output from NXP fusion library; the red line is output from a commercial inclinometer. The output from NXP lib. somewhat goes to a point&amp;nbsp; far away from real position. In other cases it tracks the red line closely. I tested my custom hardware with another algorithm to verify it; I had no problem with it.&lt;/P&gt;&lt;P&gt;I used NXP 6D Acc+Gyro algorithm for testing. The NXP lib fusion rate and sensor sampling rate is 200Hz. I also tried with 400Hz sampling rate but no change. May a software defect exist which cause&amp;nbsp;incorrect&amp;nbsp;output in the NXP Sensor Fusion algorithm?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:45:28 GMT</pubDate>
    <dc:creator>tmctwo</dc:creator>
    <dc:date>2026-02-03T23:45:28Z</dc:date>
    <item>
      <title>6D Sensor Fusion Algorithm Problem</title>
      <link>https://community.nxp.com/t5/Sensors/6D-Sensor-Fusion-Algorithm-Problem/m-p/836106#M5308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some tests&amp;nbsp;with NXP Sensor Fusion Library on my custom hardware.&amp;nbsp;The library works pretty well under most conditions. But when I move the board forward and backward in less than 1 sec - periodically to test the behaviour under vibration (especially the board in a diagonal position to the surface), sometimes I see abrupt changes at output. Please find attached the pictures. In the pictures, the blue line is output from NXP fusion library; the red line is output from a commercial inclinometer. The output from NXP lib. somewhat goes to a point&amp;nbsp; far away from real position. In other cases it tracks the red line closely. I tested my custom hardware with another algorithm to verify it; I had no problem with it.&lt;/P&gt;&lt;P&gt;I used NXP 6D Acc+Gyro algorithm for testing. The NXP lib fusion rate and sensor sampling rate is 200Hz. I also tried with 400Hz sampling rate but no change. May a software defect exist which cause&amp;nbsp;incorrect&amp;nbsp;output in the NXP Sensor Fusion algorithm?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/6D-Sensor-Fusion-Algorithm-Problem/m-p/836106#M5308</guid>
      <dc:creator>tmctwo</dc:creator>
      <dc:date>2026-02-03T23:45:28Z</dc:date>
    </item>
  </channel>
</rss>