<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How does FXTH87 use BDM to debug in STOP mode? in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827624#M5278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using the FXTH87 chip for debugging. When STOP is entered into STOP1 mode, BDM is disconnected from FXTH87.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the &amp;nbsp;FXTH871X6 datasheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN class=""&gt;3.5.3 Active BDM Enabled in STOP Mode&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Entry into the ACTIVE BACKGROUND DEBUG mode from RUN mode is enabled if the ENBDM bit in BDCSCR is set. The&amp;nbsp;BDCSCR register is not memory mapped so it can only be accessed through the BDM interface by use of the BDM commands&amp;nbsp;READ_STATUS and WRITE_CONTROL. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is how to use the commands READ_STATUS and WRITE_CONTROL to enable ENBDM?&lt;/P&gt;&lt;P&gt;I am using codewarrior10.7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:04:31 GMT</pubDate>
    <dc:creator>lison0103</dc:creator>
    <dc:date>2026-02-03T22:04:31Z</dc:date>
    <item>
      <title>How does FXTH87 use BDM to debug in STOP mode?</title>
      <link>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827624#M5278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using the FXTH87 chip for debugging. When STOP is entered into STOP1 mode, BDM is disconnected from FXTH87.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the &amp;nbsp;FXTH871X6 datasheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN class=""&gt;3.5.3 Active BDM Enabled in STOP Mode&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Entry into the ACTIVE BACKGROUND DEBUG mode from RUN mode is enabled if the ENBDM bit in BDCSCR is set. The&amp;nbsp;BDCSCR register is not memory mapped so it can only be accessed through the BDM interface by use of the BDM commands&amp;nbsp;READ_STATUS and WRITE_CONTROL. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is how to use the commands READ_STATUS and WRITE_CONTROL to enable ENBDM?&lt;/P&gt;&lt;P&gt;I am using codewarrior10.7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827624#M5278</guid>
      <dc:creator>lison0103</dc:creator>
      <dc:date>2026-02-03T22:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: How does FXTH87 use BDM to debug in STOP mode?</title>
      <link>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827625#M5279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I see the &amp;nbsp;FXTH871X6 datasheet,&amp;nbsp;Chapter 15 develoment support:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76525i0C8681F8265EC50F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to use it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 02:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827625#M5279</guid>
      <dc:creator>lison0103</dc:creator>
      <dc:date>2018-10-25T02:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: How does FXTH87 use BDM to debug in STOP mode?</title>
      <link>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827626#M5280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lison,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To enable the active background debug, this is done by default when using the target FXTH870000 (default TPMS target) in the latest CodeWarrior version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest CW version (CW11) can be installed from &lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-tools/downloads:CW_DOWNLOADS"&gt;here&lt;/A&gt; for free using the special edition (CW for MCUs Eclipse IDE, special edition).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the debug session is nonetheless disconnected when using CW11 and the target FXTH870000, it may be due to a bad hardware connection (USB cable going from the computer to the multilink, or ribbon cable from the multilink to the FXTH), or to a reset due to an instruction problem in the code (for example jump to a wrong address).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m pending to provide more information about the use of READ_STATUS and WRITE_CONTROL once I have it from internal support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the delayed response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 20:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827626#M5280</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2018-11-28T20:27:44Z</dc:date>
    </item>
    <item>
      <title>Re: How does FXTH87 use BDM to debug in STOP mode?</title>
      <link>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827627#M5281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lison,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have received confirmation from our AE. The ENBDM is enabled by default when using the latest version of CodeWarrior.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can be helpful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paulina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2018 03:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/How-does-FXTH87-use-BDM-to-debug-in-STOP-mode/m-p/827627#M5281</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2018-12-14T03:12:12Z</dc:date>
    </item>
  </channel>
</rss>