<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックFXOS8700 SPI Woes</title>
    <link>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821249#M5259</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to use the FXOS8700 in SPI mode due to the faster read / write times associated with SPI (higher possible bus speed). I have set up the SPI bus to run with the following parameters which are consistent with the FXOS8700 data sheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;CLK: 1 MHz&lt;/P&gt;&lt;P&gt;Order: MSB First&lt;/P&gt;&lt;P&gt;CPOL: Rising/Falling&lt;/P&gt;&lt;P&gt;CPHA: Sample/Setup&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified the above settings on an oscilloscope so I know that the bus is set up correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to get the FXOS into SPI mode, I tri-state the MISO pin before toggling the reset pin, and waiting the required time for the auto detection circuit to put the device into SPI mode. I then attempt to read the WHO_AM_I register and get the value 0x1e instead of 0xc7 which is what I would expect. Below is the code I am using to reset the device and read the WHO_AM_I register:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;DIV&gt;&lt;DIV&gt;#define FXOS_MISO&amp;nbsp;&amp;nbsp; 26&lt;BR /&gt;#define FXOS_CS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11&lt;BR /&gt;#define FXOS_RST&amp;nbsp;&amp;nbsp;&amp;nbsp; 3&lt;BR /&gt;void FXOSSPI()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Tri-state MISO&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinMode( FXOS_MISO, TRI_STATE );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; delay( 10 );&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reset the FXOS&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_RST, HIGH );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_RST, LOW );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; delay( 1 );&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up the bus&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPISettings _settings = SPISettings( 1000000, MSBFIRST, SPI_MODE0 );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1.beginTransaction( _settings );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read WHO_AM_I&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t tx[3] = { ( 0x0D &amp;gt;&amp;gt; 1 ) &amp;amp; 0xFF, ( 0x0D &amp;lt;&amp;lt; 7 ) &amp;amp; 0xFF , 0xFF };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_CS, LOW );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for( uint8_t i = 0; i &amp;lt; 3; i++)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; buff[i] = SPI1.transfer( tx[i] );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_CS, HIGH );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1.end();&lt;BR /&gt;}&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I run that function I check the contents of buff using a break point and ICD, the contents of buff are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;buff[0] = 0xFF&lt;/P&gt;&lt;P&gt;buff[1] = 0xFF&lt;/P&gt;&lt;P&gt;buff[2] = 0x1E&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, bytes 0, and 1 are DC because we are writing the R/W bits and the register address, but byte 2 should be 0xC7.&amp;nbsp; Not really sure what is going on here, I have looked at this many times under a scope, verified SPI register settings via ICD, slowed down the clock rate, etc. Still get the same results. Anybody else getting this problem? The only thing I can think of now is that my FXOS is damaged or something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:02:56 GMT</pubDate>
    <dc:creator>warren1</dc:creator>
    <dc:date>2026-02-03T21:02:56Z</dc:date>
    <item>
      <title>FXOS8700 SPI Woes</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821249#M5259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to use the FXOS8700 in SPI mode due to the faster read / write times associated with SPI (higher possible bus speed). I have set up the SPI bus to run with the following parameters which are consistent with the FXOS8700 data sheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;CLK: 1 MHz&lt;/P&gt;&lt;P&gt;Order: MSB First&lt;/P&gt;&lt;P&gt;CPOL: Rising/Falling&lt;/P&gt;&lt;P&gt;CPHA: Sample/Setup&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified the above settings on an oscilloscope so I know that the bus is set up correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to get the FXOS into SPI mode, I tri-state the MISO pin before toggling the reset pin, and waiting the required time for the auto detection circuit to put the device into SPI mode. I then attempt to read the WHO_AM_I register and get the value 0x1e instead of 0xc7 which is what I would expect. Below is the code I am using to reset the device and read the WHO_AM_I register:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;DIV&gt;&lt;DIV&gt;#define FXOS_MISO&amp;nbsp;&amp;nbsp; 26&lt;BR /&gt;#define FXOS_CS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11&lt;BR /&gt;#define FXOS_RST&amp;nbsp;&amp;nbsp;&amp;nbsp; 3&lt;BR /&gt;void FXOSSPI()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Tri-state MISO&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinMode( FXOS_MISO, TRI_STATE );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; delay( 10 );&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reset the FXOS&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_RST, HIGH );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_RST, LOW );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; delay( 1 );&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up the bus&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPISettings _settings = SPISettings( 1000000, MSBFIRST, SPI_MODE0 );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1.beginTransaction( _settings );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read WHO_AM_I&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t tx[3] = { ( 0x0D &amp;gt;&amp;gt; 1 ) &amp;amp; 0xFF, ( 0x0D &amp;lt;&amp;lt; 7 ) &amp;amp; 0xFF , 0xFF };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_CS, LOW );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for( uint8_t i = 0; i &amp;lt; 3; i++)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; buff[i] = SPI1.transfer( tx[i] );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; digitalWrite( FXOS_CS, HIGH );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1.end();&lt;BR /&gt;}&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I run that function I check the contents of buff using a break point and ICD, the contents of buff are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;buff[0] = 0xFF&lt;/P&gt;&lt;P&gt;buff[1] = 0xFF&lt;/P&gt;&lt;P&gt;buff[2] = 0x1E&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, bytes 0, and 1 are DC because we are writing the R/W bits and the register address, but byte 2 should be 0xC7.&amp;nbsp; Not really sure what is going on here, I have looked at this many times under a scope, verified SPI register settings via ICD, slowed down the clock rate, etc. Still get the same results. Anybody else getting this problem? The only thing I can think of now is that my FXOS is damaged or something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821249#M5259</guid>
      <dc:creator>warren1</dc:creator>
      <dc:date>2026-02-03T21:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 SPI Woes</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821250#M5260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Warren,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I found where the problem is. You are not addressing the WHO_AM_I register (0x0D) correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As shown in the datasheet:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0]&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Byte 1: ADDR[7], X, X, X, X, X, X, X&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In your case tx[0] = ( 0x0D &amp;gt;&amp;gt; 1 ) &amp;amp; 0xFF while the correct way is &lt;STRONG&gt;tx[0] = 0x0D &amp;amp; 0x7F&lt;/STRONG&gt;. Similarly tx[1] = ( 0x0D &amp;lt;&amp;lt; 7 ) &amp;amp; 0xFF while the correct form is&amp;nbsp;&lt;STRONG&gt;tx[1] = 0x0D &amp;amp; 0x80&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my complete read a register function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;/******************************************************************************
* Read a byte from the FXOS8700CQ
* 
* Byte 0: 0,ADDR[6],ADDR[5],ADDR[4],ADDR[3],ADDR[2],ADDR[1],ADDR[0]
* Byte 1: ADDR[7],0,0,0,0,0,0,0
* Byte 2: 0,0,0,0,0,0,0,0
******************************************************************************/&lt;/SPAN&gt; 
&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FXOS8700CQ_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; RegisterAddress&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; i&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
 CS_Enable&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPTEF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 SPI0_D &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x7F&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; RegisterAddress&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPRF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 i &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SPI0_D&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
 
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPTEF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 SPI0_D &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; RegisterAddress&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPRF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 i &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SPI0_D&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPTEF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 SPI0_D &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Dummy byte&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI0_S &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; SPI_S_SPRF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 i &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SPI0_D&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
CS_Disable&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 
 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; i&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 11:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821250#M5260</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-07-18T11:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 SPI Woes</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821251#M5261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't believe I missed that! Just goes to show the value of having a fresh set of eyes on your code. Thank you, everything is working as planned now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Warren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 17:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821251#M5261</guid>
      <dc:creator>warren1</dc:creator>
      <dc:date>2018-07-18T17:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 SPI Woes</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821252#M5262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are very welcome, Warren.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very glad to hear it is working now!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 08:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-SPI-Woes/m-p/821252#M5262</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-07-19T08:46:40Z</dc:date>
    </item>
  </channel>
</rss>