<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックNXP MPXV5050 Vacuum sensor support</title>
    <link>https://community.nxp.com/t5/Sensors/NXP-MPXV5050-Vacuum-sensor-support/m-p/815656#M5222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use the NXP MPXV5050GC6U to measure the vacuum level inside a box, where the levels can be in between 30milibar to 400milibar.&lt;/P&gt;&lt;P&gt;Is this the correct part to use, or there is another recommended part ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the support !&lt;/P&gt;&lt;P&gt;Kobi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:33:57 GMT</pubDate>
    <dc:creator>kobi1</dc:creator>
    <dc:date>2026-02-03T22:33:57Z</dc:date>
    <item>
      <title>NXP MPXV5050 Vacuum sensor support</title>
      <link>https://community.nxp.com/t5/Sensors/NXP-MPXV5050-Vacuum-sensor-support/m-p/815656#M5222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use the NXP MPXV5050GC6U to measure the vacuum level inside a box, where the levels can be in between 30milibar to 400milibar.&lt;/P&gt;&lt;P&gt;Is this the correct part to use, or there is another recommended part ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the support !&lt;/P&gt;&lt;P&gt;Kobi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP-MPXV5050-Vacuum-sensor-support/m-p/815656#M5222</guid>
      <dc:creator>kobi1</dc:creator>
      <dc:date>2026-02-03T22:33:57Z</dc:date>
    </item>
    <item>
      <title>Re: NXP MPXV5050 Vacuum sensor support</title>
      <link>https://community.nxp.com/t5/Sensors/NXP-MPXV5050-Vacuum-sensor-support/m-p/815657#M5223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kobi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPXV5050GC6U is a positive gauge pressure sensor, so it measures the positive pressure (up to 50 kPa) relative to the ambient pressure on the P2 side.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For your application I would recommend either absolute or negative gauge pressure sensors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The minimum rated pressure of NXP absolute pressure sensors is typically 15 kPa, so they will not respond in the range of 30 mbar to 150 mbar.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The only NXP device I can recommend is the &lt;A href="https://www.nxp.com/docs/en/data-sheet/MPXV6115V.pdf"&gt;MPXV6115VC6U&lt;/A&gt; which is a negative gauge pressure sensor designed to measure „vacuum“ from 0 kPa down to -115 kPa:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69146i108ED1AED892A2D2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 10:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NXP-MPXV5050-Vacuum-sensor-support/m-p/815657#M5223</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-09-12T10:33:50Z</dc:date>
    </item>
  </channel>
</rss>