<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: FXAS Gyro Zero Offset</title>
    <link>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812073#M5201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shubhadip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was doing exactly what you said, but without the spinning several times.&amp;nbsp; I will try that to see how it works.&amp;nbsp; Thank you for the suggestion.&amp;nbsp; I am using the sensor with the IC mounted on a board which is vertical.&amp;nbsp; The Z axis is horizontal in my application.&amp;nbsp; I don't know whether that has an impact on what I get out of the X axis. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because I don't have any of the other sensors, I didn't try to dig into the sensor fusion software.&amp;nbsp; That can come later if it becomes required, along with a re-spin to add at least an accelerometer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jul 2018 11:27:03 GMT</pubDate>
    <dc:creator>andyvoss</dc:creator>
    <dc:date>2018-07-05T11:27:03Z</dc:date>
    <item>
      <title>FXAS Gyro Zero Offset</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812071#M5199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In a system with only a gyro, what is the best way to compensate for zero offset?&amp;nbsp; I have tried a number of ways to collect measurements for a number of seconds, and then determine the resting angle rate, and then apply that to each measurement for correction.&amp;nbsp; There is always a remaining angle rate which I haven't succeeded in compensating out.&amp;nbsp; What am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/gyroscope bias estimation/tg-p" target="_blank"&gt;#gyroscope bias estimation&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812071#M5199</guid>
      <dc:creator>andyvoss</dc:creator>
      <dc:date>2026-02-03T21:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS Gyro Zero Offset</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812072#M5200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The most simple method of computing GYRO offset is spinning several times and then taking an average of at-rest numbers. I assume this is what you are doing but you are not satisfied with the result. Using the above method the bulk of the error should have been removed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How much residual error are you seeing? This&amp;nbsp;may be an orientation-dependent offset and require an Accel/Mag for further correction. You may refer to NXP Sensor Fusion, in which&amp;nbsp;the gyro offset is computed automatically and the Kalman filter should indicate the output. However, please note that NXP's&amp;nbsp;algorithm uses all available sensors and the Code for the algorithm is not&amp;nbsp;trivial and requires detailed understanding.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 18:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812072#M5200</guid>
      <dc:creator>shubhadippaul-b</dc:creator>
      <dc:date>2018-06-25T18:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS Gyro Zero Offset</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812073#M5201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shubhadip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was doing exactly what you said, but without the spinning several times.&amp;nbsp; I will try that to see how it works.&amp;nbsp; Thank you for the suggestion.&amp;nbsp; I am using the sensor with the IC mounted on a board which is vertical.&amp;nbsp; The Z axis is horizontal in my application.&amp;nbsp; I don't know whether that has an impact on what I get out of the X axis. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because I don't have any of the other sensors, I didn't try to dig into the sensor fusion software.&amp;nbsp; That can come later if it becomes required, along with a re-spin to add at least an accelerometer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 11:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812073#M5201</guid>
      <dc:creator>andyvoss</dc:creator>
      <dc:date>2018-07-05T11:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: FXAS Gyro Zero Offset</title>
      <link>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812074#M5202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shubhadip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more update.&amp;nbsp; Motion prior to collecting data while stationary does seem to help a little, but more accuracy was gained (using motion or without) by extending the sampling time.&amp;nbsp; I now sample for 30 sec which greatly improved accuracy of the calculated bias factor.&amp;nbsp; I observe that there is a low-frequency component of the bias which needs some time to be collected in the summation for the bias factor.&amp;nbsp; Thank you for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 13:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXAS-Gyro-Zero-Offset/m-p/812074#M5202</guid>
      <dc:creator>andyvoss</dc:creator>
      <dc:date>2018-07-05T13:08:59Z</dc:date>
    </item>
  </channel>
</rss>