<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックFXOS8700CQ pulse detection</title>
    <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-pulse-detection/m-p/778776#M5031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get double-tap detection to work properly. I think the data sheet is a little unclear. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the treshold values (PULSE_THSX/Y/Z) absolute values or differential values? Depending on orientation there will be a static value between -1g and +1g. The tap comes on top of that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The time steps in table 135 and 136 refers to HP_FILTER_CUTOFF[pls_hpf_en] = 0 or 1. However, the HP_FILTER_CUTOFF doesn't have a pls_hpf_en bit. It has bits pulse_hpf_byp&amp;nbsp; and pulse_lpf_en. I can't find any description what these two bits are doing. Why would you want low pass filter for pulse detection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:48:44 GMT</pubDate>
    <dc:creator>kurtmirdell</dc:creator>
    <dc:date>2026-02-03T22:48:44Z</dc:date>
    <item>
      <title>FXOS8700CQ pulse detection</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-pulse-detection/m-p/778776#M5031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get double-tap detection to work properly. I think the data sheet is a little unclear. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the treshold values (PULSE_THSX/Y/Z) absolute values or differential values? Depending on orientation there will be a static value between -1g and +1g. The tap comes on top of that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The time steps in table 135 and 136 refers to HP_FILTER_CUTOFF[pls_hpf_en] = 0 or 1. However, the HP_FILTER_CUTOFF doesn't have a pls_hpf_en bit. It has bits pulse_hpf_byp&amp;nbsp; and pulse_lpf_en. I can't find any description what these two bits are doing. Why would you want low pass filter for pulse detection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700CQ-pulse-detection/m-p/778776#M5031</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2026-02-03T22:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700CQ pulse detection</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-pulse-detection/m-p/778777#M5032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kurt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tap/pulse detection function can be configured to run through the high-pass filter (HPF) using the pulse_hpf_byp bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If pulse_hpf_byp = 0, the tap/pulse detection function processes high-pass filtered data, so the threshold value in PULSE_THSX/Y/Z registers should not take into account the static acceleration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If pulse_hpf_byp = 1, the tap/pulse detection function does not process high-pass filtered data (HPF is bypassed) and the threshold value needs to take into account the static acceleration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the pls_hpf_en bit, it is indeed an error, the correct bit is pulse_lpf_en in the HP_FILTER_CUTOFF register. When the low-pass filter is enabled (pulse_lpf_en = 1), the time step doubles. The LPF should help eliminate additional ringing after the tap signature is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it answers your questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 13:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700CQ-pulse-detection/m-p/778777#M5032</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-12-12T13:38:55Z</dc:date>
    </item>
  </channel>
</rss>