<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MPXH6250A6U</title>
    <link>https://community.nxp.com/t5/Sensors/MPXH6250A6U/m-p/764459#M4950</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raphael,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following information is given in the &lt;A href="https://www.nxp.com/docs/en/application-note/AN3150.pdf"&gt;AN3150&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The use of a No-Clean (NC) flux is recommended for exposed cavity components. Using pressure spray or other methods of cleaning is not recommended. If cleaning of the pcb is performed Water Soluble (WS) flux can be used, but it is recommended the component cavity to be protected by adhesive Kapton tape, vinyl cap or other means prior to the cleaning process to prevent contamination and foreign materials from being introduced into device cavity as result of cleaning processes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 May 2018 10:30:32 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2018-05-18T10:30:32Z</dc:date>
    <item>
      <title>MPXH6250A6U</title>
      <link>https://community.nxp.com/t5/Sensors/MPXH6250A6U/m-p/764458#M4949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, in the data sheet there is no information with the cleaning compatibility.&lt;/P&gt;&lt;P&gt;Is it possible to wash the component with aqueous machine ?&lt;/P&gt;&lt;P&gt;how many cycle we can clean it ?&lt;/P&gt;&lt;P&gt;wich type of cleaning we can used ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXH6250A6U/m-p/764458#M4949</guid>
      <dc:creator>raphaelleden</dc:creator>
      <dc:date>2026-02-03T22:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPXH6250A6U</title>
      <link>https://community.nxp.com/t5/Sensors/MPXH6250A6U/m-p/764459#M4950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raphael,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following information is given in the &lt;A href="https://www.nxp.com/docs/en/application-note/AN3150.pdf"&gt;AN3150&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The use of a No-Clean (NC) flux is recommended for exposed cavity components. Using pressure spray or other methods of cleaning is not recommended. If cleaning of the pcb is performed Water Soluble (WS) flux can be used, but it is recommended the component cavity to be protected by adhesive Kapton tape, vinyl cap or other means prior to the cleaning process to prevent contamination and foreign materials from being introduced into device cavity as result of cleaning processes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 10:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXH6250A6U/m-p/764459#M4950</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-05-18T10:30:32Z</dc:date>
    </item>
  </channel>
</rss>