<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MMA8451Q - Effective resolution calculation in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752395#M4846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The number of effective bits and typical noise calculated in mg RMS is actually given in tables 3, 4, 5 and 6 of the AN4075 for all possible ODR/MODS/LNOISE combinations. As you can see, it is practically 14-bit true at 1.56Hz in Hi Resolution Mode with the Low Noise bit set. As the sample rate decreases the resolution improves. The best case scenario is 14-bit true at the lowest sample rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Feb 2018 14:50:24 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2018-02-20T14:50:24Z</dc:date>
    <item>
      <title>MMA8451Q - Effective resolution calculation</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752394#M4845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I kundly ask about the effective resolution for this accelerometer model.&lt;/P&gt;&lt;P&gt;Suppose to work ad ODR=400 Hz hence BW=200 Hz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the device datasheet we have a PSD=99 ug/sqrt(Hz) @ 4g scale ODR=400 Hz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the AN4075 the SNR(db) will be equal to:&lt;/P&gt;&lt;P&gt;&amp;nbsp; SNR(db)=20*log*(4g/(2sqrt(2)) / NRMS)&lt;/P&gt;&lt;P&gt;where:&lt;/P&gt;&lt;P&gt;&amp;nbsp; NRMS = PSD*SQRT(BW)=99u*SQRT(200)=1.4 mg&lt;/P&gt;&lt;P&gt;Hence:&lt;/P&gt;&lt;P&gt;&amp;nbsp; SNR(db)=60.087 dB&lt;/P&gt;&lt;P&gt;and finally we have for the bits number:&lt;/P&gt;&lt;P&gt;&amp;nbsp; n=(SNR(dB)-1.76)/6.02=9.68 bit&lt;/P&gt;&lt;P&gt;This means that instead of the theoretical 14 bit we have really usable 9 bit of resolution then 4g/2^9.68=4.87 mg of resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone have carried out similar calculation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752394#M4845</guid>
      <dc:creator>bytemanaccel</dc:creator>
      <dc:date>2026-02-03T21:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q - Effective resolution calculation</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752395#M4846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The number of effective bits and typical noise calculated in mg RMS is actually given in tables 3, 4, 5 and 6 of the AN4075 for all possible ODR/MODS/LNOISE combinations. As you can see, it is practically 14-bit true at 1.56Hz in Hi Resolution Mode with the Low Noise bit set. As the sample rate decreases the resolution improves. The best case scenario is 14-bit true at the lowest sample rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 14:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752395#M4846</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-02-20T14:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q - Effective resolution calculation</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752396#M4847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;thank you for your answer, hence the best mode is on the first row of table Table 4 for a setting of 4g -&amp;gt; 14.7 bit with ODR=1.56.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 15:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-Effective-resolution-calculation/m-p/752396#M4847</guid>
      <dc:creator>bytemanaccel</dc:creator>
      <dc:date>2018-02-20T15:39:15Z</dc:date>
    </item>
  </channel>
</rss>