<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPL3115A2, I2C  pull up in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741189#M4767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok ，thank you。 What the function of VDDIO？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 08:02:56 GMT</pubDate>
    <dc:creator>owlowner</dc:creator>
    <dc:date>2018-06-13T08:02:56Z</dc:date>
    <item>
      <title>MPL3115A2, I2C  pull up</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741187#M4765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPL3115A2,Dose I2C need an external pull up voltage？or it has been pulled up inside by VDDIO？And can you give an advise for pull up resistance？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741187#M4765</guid>
      <dc:creator>owlowner</dc:creator>
      <dc:date>2026-02-03T22:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2, I2C  pull up</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741188#M4766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, external pull ups should be applied to I2C lines for MPL3115. Suggested value is 4.7k.&lt;/P&gt;&lt;P&gt;Please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/downloads/en/schematics/FRDMSTBC-P3115-SCH.pdf"&gt;FRDMSTBC-P3115-SCH&lt;/A&gt;&amp;nbsp;for a reference connection setup of MPL3115.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jun 2018 05:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741188#M4766</guid>
      <dc:creator>shubhadippaul-b</dc:creator>
      <dc:date>2018-06-03T05:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2, I2C  pull up</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741189#M4767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok ，thank you。 What the function of VDDIO？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 08:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741189#M4767</guid>
      <dc:creator>owlowner</dc:creator>
      <dc:date>2018-06-13T08:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2, I2C  pull up</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741190#M4768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Polo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VDD is the main power supply for all internal analog and digital functional blocks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;VDDIO is a separate power supply pin used for the supply of the I2C digital communication interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So VDDIO sets the interface voltage level for the MPL3115A2 and your MCU. For single-supply operation, VDDIO can be the same as the main supply VDD. In a dual-supply applications, however, VDDIO can differ from VDD to accommodate the desired interface voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let us know if you have any other questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 08:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-I2C-pull-up/m-p/741190#M4768</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-06-13T08:48:29Z</dc:date>
    </item>
  </channel>
</rss>