<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPL3115A2 accuracy clarification in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPL3115A2-accuracy-clarification/m-p/713388#M4589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i would like some help to&amp;nbsp;clarify the +- .4kPa absolute accuracy parameter in the MPL3115A2 data sheet: has this accuracy to be intended as an offset error which stays constant over the whole measurement range?&amp;nbsp;I need to measure not an absolute pressure but pressure intervals&amp;nbsp;over time, so,&amp;nbsp;on reading P1 and P2, i wouldn't mind an offset &amp;nbsp;error, as long as it&amp;nbsp;stays constant for both readings, cancelling itself out&amp;nbsp;during the calculations. Conversely,&amp;nbsp;a variable uncertainty (of &amp;nbsp;-.4 to + .4 kPa)&amp;nbsp;on every reading wouldn't be acceptable. So, is the true pressure accuracy for differential readings the +-.05 kPa stated on the data sheet? Is the "pressure absolute accuracy" an offset error,&amp;nbsp;constant&amp;nbsp;over the rated pressure range?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Daniele Paesani&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS I am aware that other sensor with different ranges/methods may seem to&amp;nbsp;be better suited for this application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:23:46 GMT</pubDate>
    <dc:creator>danielepaesani</dc:creator>
    <dc:date>2026-02-03T21:23:46Z</dc:date>
    <item>
      <title>MPL3115A2 accuracy clarification</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-accuracy-clarification/m-p/713388#M4589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i would like some help to&amp;nbsp;clarify the +- .4kPa absolute accuracy parameter in the MPL3115A2 data sheet: has this accuracy to be intended as an offset error which stays constant over the whole measurement range?&amp;nbsp;I need to measure not an absolute pressure but pressure intervals&amp;nbsp;over time, so,&amp;nbsp;on reading P1 and P2, i wouldn't mind an offset &amp;nbsp;error, as long as it&amp;nbsp;stays constant for both readings, cancelling itself out&amp;nbsp;during the calculations. Conversely,&amp;nbsp;a variable uncertainty (of &amp;nbsp;-.4 to + .4 kPa)&amp;nbsp;on every reading wouldn't be acceptable. So, is the true pressure accuracy for differential readings the +-.05 kPa stated on the data sheet? Is the "pressure absolute accuracy" an offset error,&amp;nbsp;constant&amp;nbsp;over the rated pressure range?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Daniele Paesani&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS I am aware that other sensor with different ranges/methods may seem to&amp;nbsp;be better suited for this application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-accuracy-clarification/m-p/713388#M4589</guid>
      <dc:creator>danielepaesani</dc:creator>
      <dc:date>2026-02-03T21:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 accuracy clarification</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-accuracy-clarification/m-p/713389#M4590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the absolute pressure accuracy of&amp;nbsp;± 400 Pa is an offset error within the pressure range from 50 to 110 kPa and over the specified temperature range.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Take a closer look at chapter 6 of the &lt;A href="http://www.nxp.com/docs/en/application-note/AN4528.pdf"&gt;AN4528&lt;/A&gt; describing this in more detail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 08:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-accuracy-clarification/m-p/713389#M4590</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-09-04T08:55:33Z</dc:date>
    </item>
  </channel>
</rss>